I am using STM32F030C6T6
I am unable to configure usart1 in the code. None of the registers get configured for usart1 below is the code Please Help.
I am using Standard Peripheral Libraries.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-29 12:19 AM
void RCC_Configuration(void)
{
RCC_DeInit();
//RCC_AdjustHSICalibrationValue(0x00);
RCC_HSICmd(ENABLE);
while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET)
{;}
//PLL out = (8M/2)*12 = 48 MHz
RCC_PLLConfig(RCC_PLLSource_HSI_Div2,RCC_PLLMul_12);
RCC_PLLCmd(ENABLE);
while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)
{;}
FLASH_PrefetchBufferCmd(ENABLE);
FLASH_SetLatency(FLASH_Latency_1);
//SYSclk = PLL clk
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
while(RCC_GetSYSCLKSource() != 0x08)//if PLL used as system clock
{;}
//HCLK = SYSCLK/1=48MHz
RCC_HCLKConfig(RCC_SYSCLK_Div1);
RCC_PCLKConfig(RCC_HCLK_Div1);//48MHz
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOC, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOF, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
}
////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////
void USART_Config(void)
{
USART_DeInit(USART1);
RCC_APB2PeriphResetCmd(RCC_APB2Periph_USART1, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_0);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_0);
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_Level_3;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Pin = TX_485_PIN;
GPIO_Init(TX_485_PORT, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = RX_485_PIN;
GPIO_Init(RX_485_PORT, &GPIO_InitStructure);
USART_OverSampling8Cmd(USART1, DISABLE);
USART_OneBitMethodCmd (USART1, DISABLE);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
// USART enable
USART_Cmd(USART1, ENABLE);
USART_ITConfig(USART1,USART_IT_TXE , DISABLE);
USART_ITConfig(USART1,USART_IT_RXNE , ENABLE);
USART_ITConfig(USART1,USART_IT_TC , ENABLE);
}
- Labels:
-
RCC
-
STM32F0 Series
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-29 1:04 AM
Are you strapped to using the standard peripheral library, why not use STM32CubeMX? We also have HAL based examples for a similar MCU here: STM32CubeF0/Projects/STM32F030R8-Nucleo/Examples/UART at master · STMicroelectronics/STM32CubeF0 · GitHub
If the registers are not being configured as you say then make sure you're are providing clock to the peripheral you're wanting to use.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-29 1:17 AM
I HAVE ENABLED
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
Some other clock have to be enabled ?
with Stmcube it works but i have to do with standard peripheral library
i am not using cube.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-29 3:18 AM
My std code use
// Enable USART clock
USART1_APBPERIPHCLOCK(USART1_CLK, ENABLE);
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-29 5:45 AM
You are holding the USART in reset, don't do that or understand the correct mechanics.​
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
‎2021-12-29 11:10 PM
Thank you For correction .I have Put Reset instruction by mistake,
now my code is working.