cancel
Showing results for 
Search instead for 
Did you mean: 

hv5812 vfd driver function table

Franksterb92
Associate III

could someone explain how this chip works this functScreenshot 2023-12-30 01-46-02.pngion table is so confusing to me 

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief II

AScha3_0-1703945057506.png

...seems not difficult, you have to make connections to: (+vpp , vdd, gnd )

- data in

- clk

- strobe

- blanking

-> blanking : hi = display off ; lo = display on.

-> clk : on lo->hi transition data is shifted in; 

-> strobe :  lo->hi transition data is stored in latch;  lo->hi->lo to store data . 

So full sequence to show a pattern is:

( set data in hi or lo , switch clk lo->hi->lo ;  ) 20 x , for 20 bits /segments ;

set strobe lo->hi->lo ; = data is on outputs (+ blanking always lo, if you dont want switch off the display)

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Thank you very much for the trust you have placed in the community with your question, but it relates to a device from a manufacturer that is not STMicroelectronics. This can also be seen in the URL on your screenshot. I suspect that the question can be better answered by that supplier.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
AScha.3
Chief II

AScha3_0-1703945057506.png

...seems not difficult, you have to make connections to: (+vpp , vdd, gnd )

- data in

- clk

- strobe

- blanking

-> blanking : hi = display off ; lo = display on.

-> clk : on lo->hi transition data is shifted in; 

-> strobe :  lo->hi transition data is stored in latch;  lo->hi->lo to store data . 

So full sequence to show a pattern is:

( set data in hi or lo , switch clk lo->hi->lo ;  ) 20 x , for 20 bits /segments ;

set strobe lo->hi->lo ; = data is on outputs (+ blanking always lo, if you dont want switch off the display)

If you feel a post has answered your question, please click "Accept as Solution".

So just Like the 74hc595 ok