cancel
Showing results for 
Search instead for 
Did you mean: 

Help implementing USB_OTG_HS for 2 CDC-ACMs

zcab911_monster
Associate III

I have been struggling trying to implement two CDC-ACMs on a NUCLEO-U5A5ZJ board on the USB_OTG_HS bus and am having great difficulty.  I have been successful getting them to appear on Device Manager, but I have been unsuccessful getting them to transmit data.  It just locks up when I send data, with no error code or failure.  I have found out how to do this using the FS USB, but there is no example or documentation for the HS_OTG HAL.  Its as if it's missing a FIFO, and I think it has to do with the following section which has essentially no documentation:

 

VOID USBX_APP_Device_Init(VOID)
{
  /* USER CODE BEGIN USB_Device_Init_PreTreatment_0 */
  /* USER CODE END USB_Device_Init_PreTreatment_0 */

  /* USB_OTG_HS init function */
  MX_USB_OTG_HS_PCD_Init();

  /* USER CODE BEGIN USB_Device_Init_PreTreatment_1 */
  HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
  HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, USBD_MAX_EP0_SIZE/4);
  HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, USBD_CDCACM_EPIN_HS_MPS/4);
  HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, USBD_CDCACM_EPINCMD_HS_MPS/4);
  /* USER CODE END USB_Device_Init_PreTreatment_1 */

  /* initialize the device controller driver*/
  _ux_dcd_stm32_initialize((ULONG)USB_OTG_HS, (ULONG)&hpcd_USB_OTG_HS);

  /* USER CODE BEGIN USB_Device_Init_PostTreatment */
  /* USER CODE END USB_Device_Init_PostTreatment */
}

 

  @B.Montanari 

1 REPLY 1
FBL
ST Employee

Hi @zcab911_monster 

I think you figured out the issue in this post by adjusting FIFOs initialization.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL