2023-11-03 3:01 AM
In RM 0481 (STM32H563/H573) Rev 1, on page 444, Figure 48. Clock tree, HSI RC 64 MHz output is written as HSI (hsi_ck), whereas LSI and HSI48 outputs are named as lsi_ker_ck and hsi48_ker_ck. Since there is also a HSIDIV, and it is documented correctly (on page 471, RCC_CR register fields) mentioning hsi_ker_ck, I believe on the Figure 48, hsi_ck should be renamed to hsi_ker_ck.
Solved! Go to Solution.
2023-11-06 6:45 AM
Hello again
As you can see in the page 455 of the RM0481, We have 2 different paths for the HSI output. One for the system clock which is the hsi_ck. And one for the peripheral kernel clock which is the hsi_ker_ck.
Best reagrds.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-05 11:28 AM
Hello @mete and welcome to the ST Community :smiling_face_with_smiling_eyes:.
Thank you for your post. I'm checking this internally and I will get back to you as soon as possible.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-06 6:45 AM
Hello again
As you can see in the page 455 of the RM0481, We have 2 different paths for the HSI output. One for the system clock which is the hsi_ck. And one for the peripheral kernel clock which is the hsi_ker_ck.
Best reagrds.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-11-06 6:53 AM
Thanks, yes I realized both are used, so renaming the HSI output in the figure would be wrong. However, I still think it would be good to show this on the figure both for HSI and CSI. It is a bit confusing some (HSI48) outputs _ker some doesnt (HSI and CSI) but then _ker is used in other places (peripherals).
2023-11-09 3:33 AM
Just want to add that the reason for my question was mainly because I thought HSIDIV only works for hsi_ker_ck (I thought hsi_ck is the output before HSIDIV). I realized HSIDIV is active for both, so actually, I think, there is no way to get the HSI RC output before HSIDIV, so hsi_ck and hsi_ker_ck always have the same freq. I still think it would be a good idea to add HSIDIV to the clocktree (like other prescalers).