2021-11-18 2:53 AM
MCU: STM32F407VGT discovery board
i am trying to use the stm32f407 device in low power mode. and
i go through with datasheet related to low power mode. i did not get understand.
anyone please help me how to use stm32f4 in low power mode.
2021-11-18 4:56 AM
There should be SLEEP and STANDBY examples under the CubeF4 trees for this and other boards. Look at PWR and RTC forks.
You'll probably need to add the LSE crystal and parts to the board to allow the RTC to run in low power mode.
The board also has a lot of ancillary parts that probably won't help achieve "low power" operation in the measurable sense
2021-11-18 5:12 AM
i am using HSE for RTC
2021-11-18 5:17 AM
I doubt that's going to work in STANDBY.
The simplists low power method is to use __WFI() in an idle loop.