2022-04-05 11:16 PM
I am using the B-L475E-IOT01A kit, but I am not able to find any BLE scanning example. I want to detect beacons around me and their details as well i.e RSSI, etc.
Can anyone help me regarding this?
2022-04-06 6:53 AM
I am using aci_gap_start_observation_procedure() api in place of aci_gap_create_connection() in STM32L4_IOT_P2P_ClientServer example, I have enabled LB_CLIENT = 1 .
I am getting a 0x0c error which is ERR_COMMAND_DISALLOWED.
What should the API sequence before calling aci_gap_start_observation_procedure()?
Winfred LU Can you please help me regarding this?
2022-04-10 10:36 PM
It is not allowed possibly because some other procedure is ongoing.
The sequence would be initialize firstly and it is good for observing:
When you are done the observation, terminate it by calling aci_gap_terminate_gap_procedure() with 0x80 in procedure_code.
2022-04-14 6:37 AM
Hello @PYada.1 ,
If your issue is solved, please select the answer as “Best�? as this will help other users to find answers faster.
Thanks
Imen