2021-01-07 12:51 AM
Hello. I have STM32F767ZI nucleo board. I have created a new project and used default setup for the nucleo board. It have automatically set up some peripherals for me
In my code, I want to print the debug messages to the console:
while (1)
{
/* USER CODE END WHILE */
HAL_Delay(1000);
printf("hello");
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}But the printf is not working. I remember doing simmilar excersise in the class and it did not require any additional setup.
Can someone help me understand how printf works and how to set it up? Do I need to dedicate USART port for it?
2022-01-24 5:48 AM
Thanks @suads and @Christophe VRIGNAUD, I got the STlink UART working.
2022-06-08 9:32 AM
Dear All.
I am using the Nucleo+F072RB (M0 grade) under CUBE IDE.
I am trying to implement the "printf" aproach of this post.
Even thought the last post of "Retarget" means very sound, at first I had implemented all aproach using "__io_putchar" and or "_write" merged into "main".
At first, I would like to know, if someone could explain, why some approach refere only to "__io_putchar" but not "_write"? And others approaches, like above, start with "_write" and jump to "__io_putchar"?
I must report that both approaches seems to work (0 compilation error), It seems like printing "somewhere" . I am using the CUBE IDE Embedded "terminal", which seems to work for simple HAL UART functions.
Second, the "retarget" implementation raises a lot of compilation error. So, I would ask to someone: for M0 (no SWV) should we swich ON/OFF any options on CUBE IDE environment? Or add some #include somewhere?
Third, Should we take some right action on "syscall.c/h" files, if we implement this "retarget" files approach?
Thanks in advance.
2024-06-07 9:40 AM
Including the \n\r in the printf string worked for me on a NUCLEO-H753ZI. Another tricky thing was that my Nucleo board arrived with the solder bridges configured for using LPUART1 outputting to Arduino pins D0/D1 despite the documentation indicating the default configuration is USART3 outputting to the STLink virutal com port.
2024-06-09 6:30 AM
There is one comment mentioned the use to fflush(stdout);
I got it working after adding it after printf(), still don't know why.