2025-09-13 1:17 AM - last edited on 2025-09-15 4:25 AM by mƎALLEm
Hello Community
For some reason, my post from yesterday did not go through and was marked as spam. I'm not interested in moaning about it right now, as I have managed to brick my custom board, designed with STM32H743XI and would be more interested in finding a way to unbrick it.
Before jumping to any conclusion, please read the post as it contains crucial info and things I have already tried, which you would like to suggest.
Some info about my setup, as mentioned earlier, it's a custom board with BOOT0 and RESET pins exposed using a switch, and there is a JTAG interface for debugging purposes, along with a SEGGER JLink. The way I managed to brick is that I accidentally pulled the RESET line while flashing a FW using Jlink, and since then, it seems memory is in locked mode, and neither Jlink nor ST-vLink is helpful in the rescue mission.
Things I have already tried and did not work... maybe I am missing something.
Right now, it feels like I am running out of options to recover from this situation. If someone can point me to any other solution or point out a mistake in what I have tried out so far, I would really appreciate the help!
PS: My other post on the same point, which is marked down as spam, had all the screenshots for reference to what I have tried so far, and I will try to upload them here if I can.
Solved! Go to Solution.
2025-10-06 1:58 AM
@mjuels, I think I have tried that too, but it's been quite a while, so I will try what you've suggested and share the outcome.
@Pavel A., this is not the first time a ST32H743 has been bricked for me, as I have mentioned, usually it's easy to recover from this situation using one of the suggestions or using the 'SEGGER STM32 Unlock' utility. In my case, this usually happens when trying to flash a FW using a SEGGER JLink device, and the RESET line is pulled by accident.
@AScha.3 yes, your feeling was right in my case, unfortunately. I believe in trying until the last hope dies. In my experience with STM32H743, it has been easy to recover in most cases. Will dig deeper in case I can find what exactly caused this, will share the knowledge if I find something concrete.
Thank you guys for coming up with different options and helping me in this matter, much appreciated.
PS: @AScha.3 & @Pavel A. in my case, ESD can not be the root cause, as I use an ESD (yes, grounded!) mat and wrist band while handling the device, the only thing making contact with the board was JTAG and UART cables.
2025-10-06 2:29 AM - edited 2025-10-06 2:44 AM
So in this case, sure its not damaged by ESD , last chance :
Before you give up - maybe last action: to reset the pcrop...whatever its now....
Connect to cpu , maybe using hot-plug or hardware reset, whatever works better, or at all.
So try set :
on L4xx: Uncheck PCROP_RDP + set RDP to level1 (protected) , 01 (or whatever, but NOT 0xCC !);
on H7xx: Check DMEP1 + 2 , + set RDP to level1 (protected) , 01 (or whatever, but NOT 0xCC !);
then restart/ power cycle
and then :
on L4xx: set Uncheck PCROP_RDP + RDP to 0xAA , to do regression;
on H7xx: Check DMEP1 + 2 , + RDP to 0xAA , to do regression;
L4:
H7:
then apply....
restart/ power cycle....and we know.
ed...for 'H7.
2025-10-06 2:32 AM
Yes, @AScha.3, you read my mind. I did read that in the manual, and definitely want to give it a try. Thanks for bringing it up.
2025-10-06 5:26 AM
Guess what fellas, following solution worked and STM32H743Xi is back in action again.
Run JLinkSTM32.exe to unlock the device.
The default location of this file is here: C:\Program Files\SEGGER\JLink_V796e.
This can be installed from here: https://www.segger.com/downloads/jlink/ and you need to use a jlink to do this.
PS: Funnily enough, I was using latest from the location, which was unable to unbrick it, but one of my collegue had an older version on his system and he tried and it worked like a charm!
Thank you guys for all your support! Much Appreciated!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.