2025-05-22 5:48 AM - edited 2025-05-22 5:50 AM
Stm32F746G DISCO
My program was written to accidentally flash a value to be stored in the wrong location. the display would be unresponsive so I'd reboot it without issue. My software still worked normally, it's only when it encounters that line. How I think I bricked it was when I ran it though debugging, that's when I couldn't connect it via st link. It would say no stm device found.
The strange thing is, I was able to connect to it via a different usb port and unbrick the device. When I ran the debugger again I bricked it the second time. How could this be?
It tells me this might not necessarily be solely a hardware issue but something in conjunction with Windows.
I've spent all night uninstalling, reinstalling drivers, fiddling with boot0 pin and bootloader, using different settings with st programmer, etc. Under normal circumstances id just buy a new board but I'm not in a position to do so, I need this urgently fixed by this weekend
2025-05-22 6:09 AM
Hold BOOT0 high during reset to recover the device. Putting a jumper between BOOT0 and VDD, then tapping the reset button, will do it. Then you can connect normally with STM32CubeProgrammer to erase flash and recover the device.
If your program writes to flash, put a HAL_Delay(1000) after reset but before doing so to avoid the debugger failing to connect.
2025-05-22 11:24 AM
If it keeps breaking it's something in your code.
As TDK suggests, put some delays after HAL_Init() or require some user interaction to trigger Flash interaction. Check you're not erasing memory containing your program.
Instrument the interaction so you can observe independently of the debugger. Make Error_Handler and HardFault_Handler output actionable data if you arrive there.
2025-05-22 11:51 AM
I can't connect to the device at all is the problem
I've tried the basic troubleshooting tips like setting boot0 to high etc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.