cancel
Showing results for 
Search instead for 
Did you mean: 

How to program STM32H755zit6?

WKUNY.1
Associate II

Hellow!I recently used STM32H755zit6 for a project, I can download the M7 code, but download the M4 code, the error will be "cannot load flash programming algorithm ! " , who can tell me what is going on? Thank you!

3 REPLIES 3
TDK
Guru

Might help if you included your IDE.

If you feel a post has answered your question, please click "Accept as Solution".
WKUNY.1
Associate II

Thank you! The IDE I use is Keil, version V5.29

Bouraoui Chemli
ST Employee

Hello @WKUNY.1​ 

Would you please check the parameter RAM of Algorithm as shown in attached file.

Also please refer to AN5286 which provides guidelines for the debug of custom applications running on the STM32H7x5/x7 microcontrollers.

Best regards

Bouraoui

0693W000000VYYnQAO.png