cancel
Showing results for 
Search instead for 
Did you mean: 

How to program stm32f401 black pill with Arduino IDE?

jstor.1the lost one
Associate II

I have a stm32f401 black pill, question is can you program it with the st linkv2 on an arduino IDE ? and if yes is there any tutorials on this subject ? I have already been able to program the blue pill with no problems using the uploaded bootloader

4 REPLIES 4
Amel NASRI
ST Employee

Hi @jstor.1the lost one​ ,

You can refer to my answer in this thread. The links provided there contains all details you need to get started with Arduino IDE for STM32 products.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

The cited link (this link) is going to nirvana!!

Hello @badiw ,

Thanks for being part of ST Community. The link has been recovered. 

Regards,
Lina 


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

You need to install a boot loader to allow CDC / MSC connectivity, for update or drag-n-drop type operation.

The button should allow USB DFU connectivity if you connect the cable whilst pressing. From there tools like DfuSe or STM32 Cube Programmer should be able to push an object file inward.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..