cancel
Showing results for 
Search instead for 
Did you mean: 

How to make the L4 series code compatible with L0. i have code on L4 series that i want to run on L0 series.

Nikhil Gayke
Associate III

I have code on L4 series that i want to run on L0 series. what are the changes and where that changes i have to make in order to make code runnable. I think with STM32 back word compatibility is there can any one guide me how to do that.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Peter BENSCH
ST Employee

You could check AN4809 Migrating between STM32L0 Series and STM32L4 Series / STM32L4+ Series microcontrollers

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Nikhil Gayke
Associate III

Thanks @Peter BENSCH​ 

i have gone through the document they have give hardware level how can i do l4 series code runnable with L0 where and in which file i have to make changes in the at the software level.

TDK
Super User

C code is generally transferrable. You haven't specified what you program does or what MCU features it uses, so it's anybody's guess as to what you need to change, if anything.

If you feel a post has answered your question, please click "Accept as Solution".
waclawek.jan
Super User

Generally, work through the hardware differences, identify piece(s) software which is (are) related to given difference, and modify that piece of software as needed.

JW

I have code C:\Users\nikhi\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-BLE1\6.2.2\Projects\Nucleo-L476RG

this project code i want to run on Nucleo-L073RZ how to do that

@TDK​ @Peter BENSCH​ @Community member​ 

Sebastien DENOUAL
ST Employee

Hi @Nikhil Gayke​ ,

Hope not too late.. or may be you already found solution since your initial post.

X-CUBE-BLE1 is a SW package compatible with CubeMX. You can easily generate code for your NUCLEO-L073.

Here attached is a GettingStarted document. This doc is of course available directly from CubeMX while using X-CUBE-BLE1 SW pack.

Regards,

Seb.