2018-12-26 9:45 PM
hello.
i want to make *.bin file for download into stm32L433 chip.
so,
i have to change below option or
i just change below check option
please give me information
thanks a lot
2018-12-27 1:19 AM
If the goal to program the flash of mcu, a bin file is a contiguous block of bytes. If you use s19 or hex file text format generated after linker step, the absolute addresses and non contiguous memory areas will be taken care of and supported by programmers tool. Generally these file are either produced by linker setting or file generator after link, regardless of toolchain brand.
2018-12-30 5:11 AM
Hello jeff.lee
With 1st method Post-Build Step):
You can invoke oblcopy command
arm-atollic-eabi-objcopy -O ihex ${BuildArtifactFileName} ${BuildArtifactFileBaseName}.hex; arm-atollic-eabi-objcopy -O binary ${BuildArtifactFileName} ${BuildArtifactFileBaseName}.bin
Or select Binary format converter into Output converter
Regard.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.