cancel
Showing results for 
Search instead for 
Did you mean: 

How to interfacing RFID with UART communication in stm32f429iit6

pshin.2
Associate II

Hello, I am using STM32F429IIT6 board . My board is customized and i have Only 6 pins that are PI1(GPIO_input), PH13(GPIO_Output),PA9(UART_Tx),PA10(UART_Rx),VCC,GND.

I want to check data through putty. But i am not able to understand how can i make it. Please help me with same. 0693W00000YAs8vQAD.jpg

3 REPLIES 3
Ulysses HERNIOSUS
ST Employee

Hello,

I don't see how your question would relate to RFID or even with ST25???

Can I remove the ST25 tag?

Regards, Ulysses

pshin.2
Associate II

what i am asking is that i want to interface RFID with STM32F429IIT6. above is the available PINS of RFID,i want to interface it to STM32 please guide with the same

what i am asking is that i want to interface RFID with STM32F429IIT6. above is the available PINS of RFID,i want to interface it to STM32 please guide with the same