2024-04-17 1:54 AM
Hello,
Sometimes I have my stm32F7 going in hardfault_handler, so for my customers I have to display on a screen the last address where the software crashed, then I can analyse which problem occure the crash. So I want to get the value "pc" (program counter) like I can see in the Fault Analyzer of stm32cubeide.
I tried many supossed solutions :
__attribute__ ((__noinline__)) void *get_pc()
{
return __builtin_return_address(0);
}
or
static __inline__ void *get_pc(void)
{
void *pc;
asm("mov %0, pc" : "=r"(pc));
return pc;
}
but it only return the value of the current function called, and not the same value as in the Fault Analyzer of stm32cubeide.
Is there a solution ?
Thank you
Solved! Go to Solution.
2024-04-18 12:31 AM
Ok for those who are intersted by a solution, I found what I wanted : get the program counter before the hardfault_handler, the same value as showed in the Fault Analyzer of stm32cubeide. I am worrking on a stm32f7 for information.
Here is the code in the function HardFault_Handler() :
// Put this struct in your ".h"
typedef struct
{
uint32_t r0;
uint32_t r1;
uint32_t r2;
uint32_t r3;
uint32_t r12;
uint32_t lr;
uint32_t pc;
uint32_t psr;
} ExceptionStackFrame;
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
uint32_t current_psp = __get_PSP();
ExceptionStackFrame *hardfault_stack_frame = (ExceptionStackFrame *)(current_psp);
uint32_t pc_value_at_fault = hardfault_stack_frame->pc;
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
/* USER CODE END W1_HardFault_IRQn 0 */
}
}
2024-04-17 2:36 AM
The PC value you are looking for is at the stack, so trick is to determine address of stack at fault handler entry, without C having disturbed that already.
@Tesla DeLorean published this - note that despite Keil in its name there's a section telling how to do this using gcc, too.
JW
2024-04-18 12:31 AM
Ok for those who are intersted by a solution, I found what I wanted : get the program counter before the hardfault_handler, the same value as showed in the Fault Analyzer of stm32cubeide. I am worrking on a stm32f7 for information.
Here is the code in the function HardFault_Handler() :
// Put this struct in your ".h"
typedef struct
{
uint32_t r0;
uint32_t r1;
uint32_t r2;
uint32_t r3;
uint32_t r12;
uint32_t lr;
uint32_t pc;
uint32_t psr;
} ExceptionStackFrame;
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
uint32_t current_psp = __get_PSP();
ExceptionStackFrame *hardfault_stack_frame = (ExceptionStackFrame *)(current_psp);
uint32_t pc_value_at_fault = hardfault_stack_frame->pc;
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
/* USER CODE END W1_HardFault_IRQn 0 */
}
}