2020-10-15 5:37 AM
Hi everyone,
I am using from STM32G4 series MCUs. In these 32G series, according to what is written in the errata sheet, there are some problems with the ADC hardware for Cut2.2 (Device Marking Y).
The workaround provided doesn't work for me.
I have 3 different MCUs.
Device markings of these:
STM32G431RB -> Z
STM32G431CBU -> Y
STM32G474RE -> Z
written on the MCU.
(NOTE: Version Z -> Cut 2.1, Version Y -> 2.2)
However, when ordering, this information is not written anywhere. My choice is Cut2.1 but I don't know how to choose it for ordering.
I'm waiting for your help.
Also, I would not expect such a problem from ST.
2020-10-16 5:33 AM
Hello @Mustafa ÇAKMAK ,
This ADC limitation was introduced only in Rev Y. New Rev X devices with corrected ADC bug should be ready next year, but unfortunately, I can't give you any target date for the moment.
I'm going to look into your question with our Marketing team and I'll come back to you as soon as I hear back from.
Imen
2020-10-16 6:49 AM
Thank you for your feedback.
I am very happy that there is a new revision and these problems will be fixed.
It will be very useful for me if the X version is coming out soon.
It will be useful to give an exact date for our planning.
2020-10-16 10:37 AM
The revision should visible on the marking (depending on the package size).
The package device marking figures available in the datasheet, are an example of topside marking orientation versus pin 1 identifier location.
The printed markings may differ depending on the supply chain.
Imen
2020-10-16 2:35 PM
2020-10-16 2:44 PM
Here, Rev code is written as "Z" next to the text ARM. Likewise, it says "Z" on the G474 chip. Rev code "Y" on G431CBU.
I am having difficulty determining the Revision code because it says below in the datasheet.
If Rev X is coming out too far I'll have to go over the MCU options.
2020-10-21 7:42 AM
Hello @Mustafa ÇAKMAK ,
For more information regarding coming Rev X released, please contact your FAE.
Imen