2021-05-17 1:15 AM
Hello everyone,
I think that I am missing some parameter in my calculation. I want to feed the clock to a microphone and I want the output clock to have a frequency of 48kHz x 64 = 3.072MHz. The 48kHz is the audio sampling freq and 64 is the decimation factor on the filter side. But I keep getting wrong frequency when I measure it with oscilloscope.
Btw, I am using Nucleo-144 STM32H743
I know the formula look like this (But somehow this is not true):
Decimation factor x Audio sampling freq = DFSDM clock source / Divider
And below are the details:
Output Clock that I want (DFSDM1_CKOUT): 3.072 MHz
Output Clock that I got (DFSDM1_CKOUT): 978 kHz
What am I missing here? And is the formula correct? I also include screenshot from MXCube.
Hope someone can help me. Thanks in advance.
Here are my codes:
//SystemClock----------------------------------------------------------------------------------------------------
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 30;
RCC_OscInitStruct.PLL.PLLP = 20;
RCC_OscInitStruct.PLL.PLLQ = 13;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV16;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
}
//MX_DFSDM1_Init----------------------------------------------------------------------------------------------------
static void MX_DFSDM1_Init(void)
{
/* USER CODE BEGIN DFSDM1_Init 0 */
/* USER CODE END DFSDM1_Init 0 */
/* USER CODE BEGIN DFSDM1_Init 1 */
/* USER CODE END DFSDM1_Init 1 */
hdfsdm1_filter0.Instance = DFSDM1_Filter0;
hdfsdm1_filter0.Init.RegularParam.Trigger = DFSDM_FILTER_SW_TRIGGER;
hdfsdm1_filter0.Init.RegularParam.FastMode = ENABLE;
hdfsdm1_filter0.Init.RegularParam.DmaMode = ENABLE;
hdfsdm1_filter0.Init.FilterParam.SincOrder = DFSDM_FILTER_FASTSINC_ORDER;
hdfsdm1_filter0.Init.FilterParam.Oversampling = 64;
hdfsdm1_filter0.Init.FilterParam.IntOversampling = 1;
if (HAL_DFSDM_FilterInit(&hdfsdm1_filter0) != HAL_OK)
{
Error_Handler();
}
hdfsdm1_channel0.Instance = DFSDM1_Channel0;
hdfsdm1_channel0.Init.OutputClock.Activation = ENABLE;
hdfsdm1_channel0.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_AUDIO;
hdfsdm1_channel0.Init.OutputClock.Divider = 16;
hdfsdm1_channel0.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
hdfsdm1_channel0.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE;
hdfsdm1_channel0.Init.Input.Pins = DFSDM_CHANNEL_FOLLOWING_CHANNEL_PINS;
hdfsdm1_channel0.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
hdfsdm1_channel0.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
hdfsdm1_channel0.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER;
hdfsdm1_channel0.Init.Awd.Oversampling = 1;
hdfsdm1_channel0.Init.Offset = 0;
hdfsdm1_channel0.Init.RightBitShift = 0x00;
if (HAL_DFSDM_ChannelInit(&hdfsdm1_channel0) != HAL_OK)
{
Error_Handler();
}
hdfsdm1_channel1.Instance = DFSDM1_Channel1;
hdfsdm1_channel1.Init.OutputClock.Activation = ENABLE;
hdfsdm1_channel1.Init.OutputClock.Selection = DFSDM_CHANNEL_OUTPUT_CLOCK_AUDIO;
hdfsdm1_channel1.Init.OutputClock.Divider = 16;
hdfsdm1_channel1.Init.Input.Multiplexer = DFSDM_CHANNEL_EXTERNAL_INPUTS;
hdfsdm1_channel1.Init.Input.DataPacking = DFSDM_CHANNEL_STANDARD_MODE;
hdfsdm1_channel1.Init.Input.Pins = DFSDM_CHANNEL_SAME_CHANNEL_PINS;
hdfsdm1_channel1.Init.SerialInterface.Type = DFSDM_CHANNEL_SPI_RISING;
hdfsdm1_channel1.Init.SerialInterface.SpiClock = DFSDM_CHANNEL_SPI_CLOCK_INTERNAL;
hdfsdm1_channel1.Init.Awd.FilterOrder = DFSDM_CHANNEL_FASTSINC_ORDER;
hdfsdm1_channel1.Init.Awd.Oversampling = 1;
hdfsdm1_channel1.Init.Offset = 0;
hdfsdm1_channel1.Init.RightBitShift = 10;
if (HAL_DFSDM_ChannelInit(&hdfsdm1_channel1) != HAL_OK)
{
Error_Handler();
}
if (HAL_DFSDM_FilterConfigRegChannel(&hdfsdm1_filter0, DFSDM_CHANNEL_1, DFSDM_CONTINUOUS_CONV_ON) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN DFSDM1_Init 2 */
/* USER CODE END DFSDM1_Init 2 */
}
//HAL_DFSDM_FilterMspInit-----------------------------------------------------------------------------
void HAL_DFSDM_FilterMspInit(DFSDM_Filter_HandleTypeDef* hdfsdm_filter)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(DFSDM1_Init == 0)
{
/* USER CODE BEGIN DFSDM1_MspInit 0 */
/* USER CODE END DFSDM1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SAI1|RCC_PERIPHCLK_DFSDM1;
PeriphClkInitStruct.PLL2.PLL2M = 25;
PeriphClkInitStruct.PLL2.PLL2N = 344;
PeriphClkInitStruct.PLL2.PLL2P = 7;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_0;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLL2;
PeriphClkInitStruct.Dfsdm1ClockSelection = RCC_DFSDM1CLKSOURCE_SYS;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
...
}
//HAL_DFSDM_ChannelMspInit--------------------------------------------------------------------------------
void HAL_DFSDM_ChannelMspInit(DFSDM_Channel_HandleTypeDef* hdfsdm_channel)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(DFSDM1_Init == 0)
{
/* USER CODE BEGIN DFSDM1_MspInit 0 */
/* USER CODE END DFSDM1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SAI1|RCC_PERIPHCLK_DFSDM1;
PeriphClkInitStruct.PLL2.PLL2M = 25;
PeriphClkInitStruct.PLL2.PLL2N = 344;
PeriphClkInitStruct.PLL2.PLL2P = 7;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_0;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOWIDE;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLL2;
PeriphClkInitStruct.Dfsdm1ClockSelection = RCC_DFSDM1CLKSOURCE_SYS;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
...
}
2021-05-17 5:02 AM
Hey, so, first, some reference :
From the second link the formula (just for the PDM mic) is : Fs = decimation * PDM_clock
What I would try is changing the source from audio clock to system clock, because audio clock actually refers to another peripheral (independent from DFDSM - first link)
2021-05-17 5:42 AM
Hello @Community member and welcome to the STM32 Community,
Have a look at this section: "DFSDM peripheral configuration tutorial", in the DFSDM application note: AN4990 "Getting started with sigma-delta digital interface on applicable STM32 microcontrollers". This will help you on the DFSDM configuration.
Imen