2023-09-08 09:13 AM
Hi!
I am playing around with some STM32CubeMX configurations for the STM32U599/U5A9-series, but I can't find any options to configure the display DSI-interface, only LTD RGB/parallel.
Are there any prerequisites that needs to be configured first in order for the DSI-option menu to show?
Thanks
Solved! Go to Solution.
2023-09-12 01:10 AM
Hello @Southbranch ,
For the STM32U5x9, the lowest pin package can support the DSI is 144-pins.
As already mentioned to check the availability of DSI feature, please refer to the datasheets DS13543 and DS13633 table 2.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-08 09:42 AM - edited 2023-09-08 09:46 AM
Hello @Southbranch ,
Could you please precise:
- Which STM32U5x9 device are you using?
- Which version of STM32CubeMX are you using?
Note that this DSI feature is not available in all STM32U5x9 MCU package, please refer to the datasheets DS13543 and DS13633 table 2.
If the DSI is available you can configured it as shown in the below figure:
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-08 09:46 AM
Hi @Southbranch ,
I can suggest 2 options to configure the DSI interface on STM32U5 devices:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-09 02:37 AM
2023-09-11 01:57 AM
Hello @Southbranch ,
The STM32CubeMX6.9.1 and DS13543 are correct. The bug is in STM32 MCU product selector - STMicroelectronics web site.
The The DSI feature isn't available in STM32U5A9VJ MCU.
I reported internally.
Thank you for bringing this issue to our attention.
Kaouthar.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-09-11 11:08 AM
I see, that explains..
Does this mean the lowest pin-count for DSI-support is 144-pins?
2023-09-12 01:10 AM
Hello @Southbranch ,
For the STM32U5x9, the lowest pin package can support the DSI is 144-pins.
As already mentioned to check the availability of DSI feature, please refer to the datasheets DS13543 and DS13633 table 2.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.