cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure 2 ADC same Channels in both adc

ggowd.1
Associate III

Hi Team,

Can I use 2 ADCs of same channel configured in same ADC PIN PA3 pin where ADC-1 is at 1KHz trigger timer in timer1 and ADC-2 at 2KHz trigger timer in timer3.

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello,

It's feasible but becarefull if the two ADC's sample the same channel at the same time. You will face some conversion disturbance due to the internal capacity of each ADC that will be set in parallel at that time. So it's recommended to use dual interleaved mode.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

2 REPLIES 2
AScha.3
Chief III

Hi,

basically : yes. 

Just try to set in Cube, what you want - if possible , you see ...

AScha3_0-1714479777300.png

 

If you feel a post has answered your question, please click "Accept as Solution".
SofLit
ST Employee

Hello,

It's feasible but becarefull if the two ADC's sample the same channel at the same time. You will face some conversion disturbance due to the internal capacity of each ADC that will be set in parallel at that time. So it's recommended to use dual interleaved mode.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.