How to boot trigger cm7 to cm4 in keil?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-08 10:43 PM
I'm implement IAP in Nucleo-H745ziq.
So. when i into application then cm7 trigger(boot) to cm4.
cm4 can't boot in keil but in stm32CubeIDE can boot.
SET_BIT(RCC->GCR, RCC_GCR_BOOT_C2);
- Labels:
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-08 11:51 PM
Hello @yolominwoo,
You need to include code in the CM7 project that enables the booting of the CM4 core using the HAL_RCCEx_EnableBootCore() function from the STM32H7 HAL library.
Ensure the right memory area is selected for the CM7 core, such as Flash at 0x08000000 for Boot address 0.
Build the CM7 project and load the binary onto the target device.
You need to configure the CM4 Project and ensure the memory area and startup code are appropriate for the CM4 core. Then, Build the CM4 project and load the binary onto the target device.
Load both CM7 and CM4 projects in Keil and start the debug session for each core. You should start the CM7 project first, which will then enable the booting of the CM4 core through the code you added. Then, start the CM4 project.
For more details and step-by-step guide, you can refer to the application notes and examples provided:
- AN5286: STM32H7x5/x7 dual-core microcontroller debugging (Using MDK-ARM section)
- AN5557: STM32H745/755 and STM32H747/757 lines dual-core architecture" (especially the section 3 Resources for dual-core application).
Hope this helped you
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 12:27 AM - edited ‎2024-05-09 12:34 AM
This doesn't work either.
I'm check already flash cm7 boot addres
HAL_RCCEx_EnableBootCore(RCC_BOOT_C2);
STM32CubeIDE Application Projcet it work cm4
But keil Application Project can't boot cm4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 12:35 AM
Please provide more details (your configuration, Cube and tools version used) and list the steps you did along with the errors you encountered, in order to be able to answer.
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 12:48 AM - edited ‎2024-05-09 12:49 AM
STM32CubeMX 6.11.1
uVision 5.38
STM32CubeIDE Last Release
I'm make a IAP for cm7 and cm4
I wish BOOT_CM4 disable. and When jump Iap to Application then Trigger for cm7 to cm4.
I'm moved stm32CubeIDE to uVision. but already can't cm4 boot.
uVision(Application CM4 main.c) Can't boot cm4
stm32CubeIDE(Application CM4 main.c) Can boot cm4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 12:57 AM - edited ‎2024-05-09 01:13 AM
If HAL_RCCEx_EnableBootCore(RCC_BOOT_C2); need shared memory?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 03:31 AM
Hi @yolominwoo ,
Can you please test this ready-to-use example within Keil:
\Repository\STM32Cube_FW_H7_V1.11.1\Projects\STM32H747I-DISCO\Applications\ResourcesManager\ResourcesManager_SharedResources
Then, please keep me informed about your update.
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-09 08:21 PM - edited ‎2024-05-12 05:16 PM
I'm tried again Today in STM32CubeIDE.
First. I'm made new Application Project.
CM7 in main.c I'm code just one line SET_BIT(RCC->GCR, RCC_GCR_BOOT_C2);
But I can't boot cm4.
However, I'm tried Changed CM7 timer TIM4 from SYSTICK
Then CM4 can boot.
You know why that worked?
Now, My Keil application project can trig boot for cm4