cancel
Showing results for 
Search instead for 
Did you mean: 

How many 32 bit timers does STM32H573 have? 2 or 4? Conflicting information in data sheet

F71334
Associate II

Hello,

I'm refering to DS14121 Rev 1 of STM32H573xx. 

- "Figure 1. STM32H573xx block diagram" shows 4 32 bit timers (TIM2, TIM3, TIM4, TIM5)

- "Table 2. STM32H573xx features and peripheral counts" says there are only two.

Where can I find trustworthy information on the correct number?

Have a nice day,

F

10 REPLIES 10

@AScha.3 wrote:

btw

Fig.1 , block diagram  has a lot of extra memory :)

 

AScha3_0-1702542325033.png

512 KB !  or 512 byte, as in text... ?? maybe STM should look here too.


Hello @AScha.3 ,

This typo is fixed in the DS14121 rev 3.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS: This is NOT an online support (https://ols.st.com) but a collaborative space. So please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help/support.