2023-02-12 11:16 AM
I have uploaded the maple bootloader and am trying to upload a sketch from the Arduino IDE (1.8.19 or 2.0.3). I get the following error:
Board identied as /dev/ttyACM0 (Maple Mini)
Upload fails:
Failed to open serial device.
setRTS(): TIOCMSET: Broken pipe
No DFU capable USB device found
dfu-util 0.7
Copyright 2005-2008 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2012 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to dfu-util@lists.gnumonks.org
Filter on vendor = 0x1eaf product = 0x0003
Waiting for /dev/ttyACM0 serial...Done
2023-02-13 12:45 AM
>>No DFU capable USB device found
Arduino needs the correct arduino bootloader to use DFU (usb flash programming).
Did you previously flashed the wrong arduino bootloader? (maybe the one for a stm32f103c8t6 bluepill?)
I would recommend you to use an STLINK, arduino supports SW (ISP as they call it) .
2023-02-13 02:09 AM
Thank you for taking the time to answer my question.
How do I know which is the correct bootloader? My understanding at this point is that the file to use it called generic_boot20_pc13.bin and is available from Roger Clarks Github. That is the one I am uploading to the board using an ST-LINKv2. That works fine, although I have discovered that the board must then be plugged directly into the PC rather than a USB hub to show up on /dev/ttyACM0.
Once the bootloader is uploaded the board shows up in the Arduino as a 'Maple Mini'. I have no idea whether this is DFU capable or not?
Since uploadfing using ST-LINKv2 works just fine, I would be happy to use that option. However where does the Arduino 'Serial' device output go? If I upload a sketch via ST-LINK-v2, the board does not appear to be accessible via the USB port or via A9/A10 as indicated on some tutorials?
2023-02-13 02:33 AM
>My understanding at this point is that the file to use it called generic_boot20_pc13.bin
Show us, post some link, are you sure your board is STM32F301C8 and not STM32F103C8?
>However where does the Arduino 'Serial' device output go?
It goes to the USB, same place
2023-02-13 02:53 AM
You are correct! Yes the board is an STM32F103C8!. My mistake in the title of the opening post which I have now corrected. I get nothing coming out of USB in terms of serial output.
2023-02-13 07:46 AM
show us a picture of your board, is there a chance is an aliexpress bluepill?
2023-02-13 08:02 AM
I don't buy from AliExpress, but that doesn't mean its not a clone. I puchased it maybe a couple of years ago from eBay. Its been sat in a box of bits ever since. The black heat-shrink covers a resistor I added as per instructions to reduce the resistance down from 10k to 1.5k.
2023-02-13 09:11 AM
Just checking, did you move the corresponding jumper when flashing the arduino bootloader in your board?
https://www.youtube.com/watch?v=Myon8H111PQ
2023-02-13 09:29 AM
the 10k was wrong on all these boards, so 10-> 1k5 is right. is only needed for USB device working mode.
+ the unknown F301 mutating to well known F103 . 🙂
so now we know, what we talking about.
you have to know: you have 3 ways to start / load new program ->
so first : choose, what you wanna do. (i use stlink always, just working...and arduino only on AVR boards)
2023-02-13 12:03 PM
I just reviewed that video and I see there is a different URL for the library. I still had the library by Dan Brown installed. I have now updated the library. I have also tried the bootloader discussed in the video, but don't even get a /dev/ttyACM0 port with hid_generic_pc13.bin...
BTW, yes I am moving the jumper to the position shown before flashing.