2019-03-27 12:57 AM
Dear forum,
I am using ST STM32F103R8T6 MCU for my medical project, i referred the hardware design guide to design the MCU schematics, now i have question in my mind that how do i deal with unused pins?
should i connect 10K resistor to ground? or
should i directly connect unused pins to ground?
i am attaching the guide which i used to design the schematics.
in this guide i did not find any statement which says how to deal with unused pins.
please help me out.
Solved! Go to Solution.
2019-03-27 1:35 AM
I suppose we should start with what you should not do. You should not leave them as digital inputs with nothing connected to them. This is because a digital input that happens to float some way between the supply lines will waste power in the digital input circuit. And wasting power is bad (ok it's not very bad in the sense that it won't catch fire, but if it is battery-powered, the battery will run out more quickly than otherwise).
So what might you do?
Program unused pins to be
I like to have some pins as digital inputs with internal pull-up. This way the same code might detect it has been put on a different pcb or has extra hardware attached if that pin is sometimes externally tied to Vss.
And other spare pins as digital outputs, that I can monitor for debugging / status purposes. Maybe even hang an LED through a resistor off here on prototype boards.
It's your choice, and there's little to choose between the "good" options.
Hope this helps,
Danish
2019-03-27 1:35 AM
I suppose we should start with what you should not do. You should not leave them as digital inputs with nothing connected to them. This is because a digital input that happens to float some way between the supply lines will waste power in the digital input circuit. And wasting power is bad (ok it's not very bad in the sense that it won't catch fire, but if it is battery-powered, the battery will run out more quickly than otherwise).
So what might you do?
Program unused pins to be
I like to have some pins as digital inputs with internal pull-up. This way the same code might detect it has been put on a different pcb or has extra hardware attached if that pin is sometimes externally tied to Vss.
And other spare pins as digital outputs, that I can monitor for debugging / status purposes. Maybe even hang an LED through a resistor off here on prototype boards.
It's your choice, and there's little to choose between the "good" options.
Hope this helps,
Danish
2019-03-27 3:42 AM
Dear Danish,
Thank you for your reply.
2019-03-27 7:41 AM
Hi @Bhat ,
Please have a look to AN4899.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.