cancel
Showing results for 
Search instead for 
Did you mean: 

How can I log (read and write) data to an SD card on an STM32L0 or L1 or any STM32 for that matter over SPI.

CAlbe.2
Associate II

I've been furiously googling for days and I can only find random libraries that people have written and most have been abandoned or are just so complex I cant get it working.

All I want to do is to log a line of data to a file on an SD card with the filename being the date. And then be able to read the file's data at a later stage.

A fairly simple task on an Arduino using their library but seemingly very difficult on an STM32. I've watched the digikey video on SPI on an STM32 which is fantastic so I have a handle on that but have no idea how to actually talk to the SD card.

I know I can program this with the Arduino IDE but the STM32 has so many capabilities that I would give up by not using CubeIDE.

Help on this would be much appreciated. I feel there should be a relatively simple solution I'm just not finding it.

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0