2024-02-04 10:48 PM - last edited on 2024-02-05 5:02 AM by mƎALLEm
To Andrew, SofLi
Hy Andrew and SofLi. I well received your last informations posted this week-end. Therefore it was week-end.
I test a NUCLEO board without ST-link; my computer is a Mac-mini and the NUCLEO board offers capabilities to be separate in to part, the ST-link microcontroller and the targeted microcontroller, enabling to reduce power consumption on plant. Bootloader offer capability to read and write any address in address space; then I think the simply way to give you understable informations it's to give you an excell file with the list of my search. Hoping this is nice to you, I hope an answer.
Best regards.
Butterfly.
Solved! Go to Solution.
2024-02-05 4:59 AM - edited 2024-02-05 5:04 AM
Found in stm32l053xx.h (located under Drivers\CMSIS\Device\ST\STM32L0xx\Include in STM32CubeL0 package) in attachment:
#define PERIPH_BASE (0x40000000UL) /*!< Peripheral base address in the alias region */
/*!< Peripheral memory map */
#define APBPERIPH_BASE PERIPH_BASE
#define AHBPERIPH_BASE (PERIPH_BASE + 0x00020000UL)
#define IOPPERIPH_BASE (PERIPH_BASE + 0x10000000UL)
#define TIM2_BASE (APBPERIPH_BASE + 0x00000000UL)
#define TIM6_BASE (APBPERIPH_BASE + 0x00001000UL)
#define LCD_BASE (APBPERIPH_BASE + 0x00002400UL)
#define RTC_BASE (APBPERIPH_BASE + 0x00002800UL)
#define WWDG_BASE (APBPERIPH_BASE + 0x00002C00UL)
#define IWDG_BASE (APBPERIPH_BASE + 0x00003000UL)
#define SPI2_BASE (APBPERIPH_BASE + 0x00003800UL)
#define USART2_BASE (APBPERIPH_BASE + 0x00004400UL)
#define LPUART1_BASE (APBPERIPH_BASE + 0x00004800UL)
#define I2C1_BASE (APBPERIPH_BASE + 0x00005400UL)
#define I2C2_BASE (APBPERIPH_BASE + 0x00005800UL)
#define CRS_BASE (APBPERIPH_BASE + 0x00006C00UL)
#define PWR_BASE (APBPERIPH_BASE + 0x00007000UL)
#define DAC_BASE (APBPERIPH_BASE + 0x00007400UL)
#define LPTIM1_BASE (APBPERIPH_BASE + 0x00007C00UL)
#define SYSCFG_BASE (APBPERIPH_BASE + 0x00010000UL)
#define COMP1_BASE (APBPERIPH_BASE + 0x00010018UL)
#define COMP2_BASE (APBPERIPH_BASE + 0x0001001CUL)
#define COMP12_COMMON ((COMP_Common_TypeDef *) COMP1_BASE)
#define EXTI_BASE (APBPERIPH_BASE + 0x00010400UL)
#define TIM21_BASE (APBPERIPH_BASE + 0x00010800UL)
#define TIM22_BASE (APBPERIPH_BASE + 0x00011400UL)
#define FIREWALL_BASE (APBPERIPH_BASE + 0x00011C00UL)
#define ADC1_BASE (APBPERIPH_BASE + 0x00012400UL)
#define ADC_BASE (APBPERIPH_BASE + 0x00012708UL)
#define SPI1_BASE (APBPERIPH_BASE + 0x00013000UL)
#define USART1_BASE (APBPERIPH_BASE + 0x00013800UL)
#define DBGMCU_BASE (APBPERIPH_BASE + 0x00015800UL)
#define DMA1_BASE (AHBPERIPH_BASE + 0x00000000UL)
#define DMA1_Channel1_BASE (DMA1_BASE + 0x00000008UL)
#define DMA1_Channel2_BASE (DMA1_BASE + 0x0000001CUL)
#define DMA1_Channel3_BASE (DMA1_BASE + 0x00000030UL)
#define DMA1_Channel4_BASE (DMA1_BASE + 0x00000044UL)
#define DMA1_Channel5_BASE (DMA1_BASE + 0x00000058UL)
#define DMA1_Channel6_BASE (DMA1_BASE + 0x0000006CUL)
#define DMA1_Channel7_BASE (DMA1_BASE + 0x00000080UL)
#define DMA1_CSELR_BASE (DMA1_BASE + 0x000000A8UL)
#define RCC_BASE (AHBPERIPH_BASE + 0x00001000UL)
#define FLASH_R_BASE (AHBPERIPH_BASE + 0x00002000UL) /*!< FLASH registers base address */
#define OB_BASE (0x1FF80000UL) /*!< FLASH Option Bytes base address */
#define FLASHSIZE_BASE (0x1FF8007CUL) /*!< FLASH Size register base address */
#define UID_BASE (0x1FF80050UL) /*!< Unique device ID register base address */
#define CRC_BASE (AHBPERIPH_BASE + 0x00003000UL)
#define TSC_BASE (AHBPERIPH_BASE + 0x00004000UL)
#define RNG_BASE (AHBPERIPH_BASE + 0x00005000UL)
#define GPIOA_BASE (IOPPERIPH_BASE + 0x00000000UL)
#define GPIOB_BASE (IOPPERIPH_BASE + 0x00000400UL)
#define GPIOC_BASE (IOPPERIPH_BASE + 0x00000800UL)
#define GPIOD_BASE (IOPPERIPH_BASE + 0x00000C00UL)
#define GPIOH_BASE (IOPPERIPH_BASE + 0x00001C00UL)
Based on that, you can add the registers' offsets.
2024-02-05 1:46 AM - edited 2024-02-05 3:24 AM
@butterfly wrote:I well received your last informations posted this week-end.
Why not continue in that thread?
Please give a link so we can find what you're referring to.
I don't wish to open unknown XLSX files from the internet - sorry.
2024-02-05 2:38 AM
Hello,
As I said in this thread https://community.st.com/t5/stm32-mcus-products/looking-for-registers-informations-to-configure-stm32l0-series/td-p/635100,
The base address of the peripherals are provided in the reference manual.
Then you compute each register absolute address based on its offset of its related peripheral.
Absolute register address = peripheral start address + register offset
Example:
FLASH_ACR address offset = 0x0000 0000
Flash registers base address 0X4002 2000
FLASH_ACR Absolute address = 0X4002 2000 + 0x0000 0000 = 0X4002 2000
2024-02-05 3:21 AM
@mƎALLEm wrote:Hello,
As I said in this thread https://community.st.com/t5/stm32-mcus-products/looking-for-registers-informations-to-configure-stm32l0-series/td-p/635100,
The forum has broken that link:
(probably due to the trailing comma?)
Try:
2024-02-05 3:23 AM
@mƎALLEm wrote:Then you compute each register absolute address based on its offset of its related peripheral.
@butterfly and, as already noted, ST provide a header file which has already done all those computations - and more - for you.
No need to re-invent the wheel!
2024-02-05 4:48 AM
Hy thanks to don't need to re-invent the wheel. In my file each register named is at an absolute address with a 0 offset. That mean for each peripheral there are different base addresses with offset for each following registers.
If you have an include file which can be part of standard delivery may I find it on a server dedicated to st-community or could you send me a copy?
Best regards.
Alain LE BLOA.
2024-02-05 4:56 AM
See your previous thread:
Again, what was the point in starting a new thread? Now you're just confusing the issue by having the discussion spread across two threads!
2024-02-05 4:59 AM - edited 2024-02-05 5:04 AM
Found in stm32l053xx.h (located under Drivers\CMSIS\Device\ST\STM32L0xx\Include in STM32CubeL0 package) in attachment:
#define PERIPH_BASE (0x40000000UL) /*!< Peripheral base address in the alias region */
/*!< Peripheral memory map */
#define APBPERIPH_BASE PERIPH_BASE
#define AHBPERIPH_BASE (PERIPH_BASE + 0x00020000UL)
#define IOPPERIPH_BASE (PERIPH_BASE + 0x10000000UL)
#define TIM2_BASE (APBPERIPH_BASE + 0x00000000UL)
#define TIM6_BASE (APBPERIPH_BASE + 0x00001000UL)
#define LCD_BASE (APBPERIPH_BASE + 0x00002400UL)
#define RTC_BASE (APBPERIPH_BASE + 0x00002800UL)
#define WWDG_BASE (APBPERIPH_BASE + 0x00002C00UL)
#define IWDG_BASE (APBPERIPH_BASE + 0x00003000UL)
#define SPI2_BASE (APBPERIPH_BASE + 0x00003800UL)
#define USART2_BASE (APBPERIPH_BASE + 0x00004400UL)
#define LPUART1_BASE (APBPERIPH_BASE + 0x00004800UL)
#define I2C1_BASE (APBPERIPH_BASE + 0x00005400UL)
#define I2C2_BASE (APBPERIPH_BASE + 0x00005800UL)
#define CRS_BASE (APBPERIPH_BASE + 0x00006C00UL)
#define PWR_BASE (APBPERIPH_BASE + 0x00007000UL)
#define DAC_BASE (APBPERIPH_BASE + 0x00007400UL)
#define LPTIM1_BASE (APBPERIPH_BASE + 0x00007C00UL)
#define SYSCFG_BASE (APBPERIPH_BASE + 0x00010000UL)
#define COMP1_BASE (APBPERIPH_BASE + 0x00010018UL)
#define COMP2_BASE (APBPERIPH_BASE + 0x0001001CUL)
#define COMP12_COMMON ((COMP_Common_TypeDef *) COMP1_BASE)
#define EXTI_BASE (APBPERIPH_BASE + 0x00010400UL)
#define TIM21_BASE (APBPERIPH_BASE + 0x00010800UL)
#define TIM22_BASE (APBPERIPH_BASE + 0x00011400UL)
#define FIREWALL_BASE (APBPERIPH_BASE + 0x00011C00UL)
#define ADC1_BASE (APBPERIPH_BASE + 0x00012400UL)
#define ADC_BASE (APBPERIPH_BASE + 0x00012708UL)
#define SPI1_BASE (APBPERIPH_BASE + 0x00013000UL)
#define USART1_BASE (APBPERIPH_BASE + 0x00013800UL)
#define DBGMCU_BASE (APBPERIPH_BASE + 0x00015800UL)
#define DMA1_BASE (AHBPERIPH_BASE + 0x00000000UL)
#define DMA1_Channel1_BASE (DMA1_BASE + 0x00000008UL)
#define DMA1_Channel2_BASE (DMA1_BASE + 0x0000001CUL)
#define DMA1_Channel3_BASE (DMA1_BASE + 0x00000030UL)
#define DMA1_Channel4_BASE (DMA1_BASE + 0x00000044UL)
#define DMA1_Channel5_BASE (DMA1_BASE + 0x00000058UL)
#define DMA1_Channel6_BASE (DMA1_BASE + 0x0000006CUL)
#define DMA1_Channel7_BASE (DMA1_BASE + 0x00000080UL)
#define DMA1_CSELR_BASE (DMA1_BASE + 0x000000A8UL)
#define RCC_BASE (AHBPERIPH_BASE + 0x00001000UL)
#define FLASH_R_BASE (AHBPERIPH_BASE + 0x00002000UL) /*!< FLASH registers base address */
#define OB_BASE (0x1FF80000UL) /*!< FLASH Option Bytes base address */
#define FLASHSIZE_BASE (0x1FF8007CUL) /*!< FLASH Size register base address */
#define UID_BASE (0x1FF80050UL) /*!< Unique device ID register base address */
#define CRC_BASE (AHBPERIPH_BASE + 0x00003000UL)
#define TSC_BASE (AHBPERIPH_BASE + 0x00004000UL)
#define RNG_BASE (AHBPERIPH_BASE + 0x00005000UL)
#define GPIOA_BASE (IOPPERIPH_BASE + 0x00000000UL)
#define GPIOB_BASE (IOPPERIPH_BASE + 0x00000400UL)
#define GPIOC_BASE (IOPPERIPH_BASE + 0x00000800UL)
#define GPIOD_BASE (IOPPERIPH_BASE + 0x00000C00UL)
#define GPIOH_BASE (IOPPERIPH_BASE + 0x00001C00UL)
Based on that, you can add the registers' offsets.
2024-02-05 5:00 AM
https://github.com/STMicroelectronics/STM32CubeL0/tree/master/Drivers/CMSIS/Device/ST click on STM32L0xx @ b3b1d7b -> Include -> https://github.com/STMicroelectronics/cmsis_device_l0/tree/b3b1d7b134f5408c3e75363754d44a6aa11b1db1/Include
You are supposed to #include "stm32l0xx.h" while having defined STM32L053xx symbol (i.e. either #define STM32L053xx before the #include; or better, -DSTM32L053xx in command-line). stm32l0xx.h will include also relevant generic-ARM CMSIS headers from https://github.com/STMicroelectronics/STM32CubeL0/tree/master/Drivers/CMSIS/Core/Include
JW
2024-02-05 5:09 AM
For the NUCLEO L053R8 board, go to the Product Page, and look under 'Tools & Software':
https://www.st.com/en/evaluation-tools/nucleo-l053r8.html#tools-software
Look at the 'MCU & MPU Embedded Software' section - the STM32CubeL0 pack will have what you need:
https://www.st.com/en/embedded-software/stm32cubel0.html