cancel
Showing results for 
Search instead for 
Did you mean: 

stm32u5 OpenOCD and stlink-server issues on macOS

larschrj
Visitor

I am trying to connect to the b-u585i-iot02a on macOS 15.3.1 using OpenOCD without success. The same board, cables and configuration scripts with the same version of OpenOCD (0.12.0+dev-01888-ga168c6341) works on both Windows 11 and Ubuntu 24.04. ST-Link server also does not work.

OpenOCD and included with STM32CubeIDE 1.18 also seem to run into the same issue so this does not seem to be specific to the official release.

The board has been updated to the latest stlink firmware (v3j16m7).

I have attached the OpenOCD -d3 log.

It might be helpful to note that I have no issues with a Nucleo-F411 board on the same macOS machine.

I would appreciate any help or advice anyone can provide.

0 REPLIES 0