2021-02-22 8:49 PM
I am using STM32F030F4P6.
VREFINT is supposed to be calibrated at 3.3v +/- 10mV and 30 degrees C. In my application the VREFINT calibration value is 1543 meaning the reference voltage is 1.243V (3.3/4096*1543) this is on the high end of the spectrum, but within limits.
When using the calbirated VREFINT, I found that my VDDA calculations were stable, but off by a bit over 1%. I have a VDDA/VDD voltage of 3.3013V measured with a calibrated multimeter (I have a DC standard to check calibration) and ambient temperature is 24.3 deg C.
Taking the average of 4000 samples from VREFINT with this setup yields a reading of 1527 or 1.230V which is bang-on specification. It is also 1.01% different to the calibrated value. How accurate should I expect the VREFINT calibration value to be? I ask because if factory calibration should be better than this, I need to find out where my design is inaccurate.
Solved! Go to Solution.
2021-03-02 2:56 AM
****** tricky error sequencing. Thanks for sharing! However I do not see a hint in the errate sheet. Did I miss the hint?
2021-03-02 4:29 AM
Dear Uwe,
I agree it lacks clarity in tracking down this issue.
It is I think linked to the fact that in parallel, we realized that the DS data for Vrefint itself were incorrect in DS, It has been associated to a F030 DS update in January 2017 and a PCI "product change information" with below descritpion (not referencing calibration correction explicitly but the VREFINT testing improvement) it was previously stated that Vrefint typ value was 1.20V:
Extract of PCI
"No change on product function nor performance.
VREFINT documentation is updated thanks to 100% production testing:
- Minimum value is improved.
- Maximum value, that was previously based on characterization, is now aligned with
production testing criteria.
- Typical value is updated accordingly."
I hope it helps explain a bit the situation.
Best regards,
Antoine
2021-03-02 3:07 PM
Hi Antoine,
Thank you for your confirmation. It is good to have an answer to the issue. I was still a little concerned that the real problem may lie elsewhere in my design, but your answer dispels any doubt. Have a good day.