Dear community members,No erase operation or RDP activation, regression should have impact on your HSI calibrated value. This calibration value is evaluated during production and stored internally on a (system) read only memory location, it is then a...
Dear Jan, Vladimir,Indeed Unique ID tend to be a feature reserved to access line and dropped in Value Line. Thank you Jan. This was partially done in our documentation, RM is aligned with strategy but not all STM32G0x0 Datasheet. This will updated in...
Hello,In fact you are not allowed to modify the option bytes themselves in Non Volatile Memory (@0x1FFF7800), you must modify there copies in the Flash interface Registers (@0x40022020) and then launch programing in the NVM by setting OPTSTRT (this w...
Hello,Sorry for long delay on this topic. There is indeed no mention of Rev 2 in errata sheet. This must be corrected rapidly.However, Rev Y and Rev 2 are controllers produced with exactly identical masks, but on 2 different production plants. (As it...
Hello Zjing, You mentioned a VDDA voltage at 3.3V in a comment, but in temperature calculation in your first post I have the impression the formula is based on a 3V supply (a 3.0 factor remains there)Best regards,Antoine