2019-11-05 02:09 AM
When the boot mode activated in STM32F427VIT6 ( BOOT0 pin to HIGH level) , the pin PE13 in strong HIGH state (really 3.3V). Why? The PE13 pin goes to LOW level just if i begin download firmware by UART bootloader
2019-11-05 04:39 AM
> ( BOOT0 pin to HIGH level) , the pin PE13 in strong HIGH state
What is connected to PE13?
Also, is it going to HIGH immediately after NRST ends? (observe with an oscilloscope).
JW
2019-11-05 05:01 AM
2019-11-05 05:18 AM
NRST is active low, at that moment all pins are Hi-Z by the processor.
So why is PE13 actually higher during NRST low, if it's just a 10k resistor to GND?
The 2.4V after reset ends is suspicious, too, though.
JW
2019-11-05 06:59 AM
Yes. its higher during NRST low... and it state of PE13 will be switch on MOSFET with current 1A in my circuit (if i connect this pin)