cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum frequency for SDMMC module when 4-bit mode is used??

Iswarya
Associate II

What is the maximum frequency for SDMMC module when 4-bit mode is used??

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Depends on a lot of factors, but most microSD cards can have wire clocks in excess of 50 MHz.

On the H7 I think I'm usually clocking the SDMMC module at 200 MHz

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Actual got data read rates a lot closer to 30 MBps in other testing, this is kind of base-line expectations:

https://community.st.com/s/question/0D50X0000BEYt8MSQT/stm32h743-stm32h7-sdmmc-dma-not-configurable

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..