cancel
Showing results for 
Search instead for 
Did you mean: 

Hi. I've included the code below. I want to pause for 10 seconds in standby mode. The code works once and never returns. And there is no serious drop in Ammeter. What could I be doing wrong?

ZKURT.1
Senior
#include <string.h>
#include <stdio.h>
#define printf(...)  HAL_UART_Transmit((UART_HandleTypeDef *)&hlpuart1, (uint8_t *)u_buf,\
		                                sprintf((char*)u_buf,__VA_ARGS__), 0xFFFF);
uint8_t u_buf[256];
/* USER CODE BEGIN 2 */
 
 
  if (__HAL_PWR_GET_FLAG(PWR_FLAG_SB) != RESET)
 	     {
 	   	  __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);  // clear the flag
 
 	   	  /** display  the string **/
 	       printf("Wakeup from the STANDBY MODE\r\n");
 
 	   	  /** Blink the LED **/
 	   	  for (int i=0; i<20; i++)
 	   	  {
 	   		  HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13);
 	   		  HAL_Delay(200);
 	   	  }
 
 	   	  /** Disable the WWAKEUP PIN **/
 	   	  HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);  // disable PA0
 
 	   	  /** Deactivate the RTC wakeup  **/
 	   	  HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
 	     }
 
 
 	     /** Now enter the standby mode **/
 	      /* Clear the WU FLAG */
 	     __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
 
 	      /* clear the RTC Wake UP (WU) flag */
 	     __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);
 
 	      /* Display the string */
 	     printf("About to enter the STANDBY MODE\r\n");
 	      /* Blink the LED */
 	     for (int i=0; i<5; i++)
 	     {
 	   	  HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_13);
 	   	  HAL_Delay(750);
 	     }
 
 	      /* Enable the WAKEUP PIN */
 	     HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
 
 	     /* enable the RTC Wakeup */
 	       /*  RTC Wake-up Interrupt Generation:
 	         Wake-up Time Base = (RTC_WAKEUPCLOCK_RTCCLK_DIV /(LSI))
 	         ==> WakeUpCounter = Wake-up Time / Wake-up Time Base
 
 	         To configure the wake up timer to 5s the WakeUpCounter is set to 0x2710:
 	         RTC_WAKEUPCLOCK_RTCCLK_DIV = RTCCLK_Div16 = 16
 	         Wake-up Time Base = 16 /(32KHz) = 0.0005 seconds
 	         ==> WakeUpCounter = ~5s/0.0005s = 20000 = 0x2710
 	       */
 	     if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0x5F46, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
 	     {
 	       Error_Handler();
 	     }
 
 	      /* one last string to be sure */
 	     printf("STANDBY MODE is ON\r\n");
 	      /* Finally enter the standby mode */
 	     HAL_PWR_EnterSTANDBYMode();
/* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
	 
 
 
  }

1 ACCEPTED SOLUTION

Accepted Solutions
ZKURT.1
Senior

The problem was the boot0 pin. Connecting the boot0 pin to gnd with a 1k resistor solved the problem. StandBy works.

View solution in original post

3 REPLIES 3
MM..1
Chief III

As first you need reconfig stlink to no debug in low power mode and turn off power to mcu .

After this flash code (no debug) and measure.Current must drop.

Second stage is wake up... read examples in firmware lib folder.

ZKURT.1
Senior

The problem was the boot0 pin. Connecting the boot0 pin to gnd with a 1k resistor solved the problem. StandBy works.