cancel
Showing results for 
Search instead for 
Did you mean: 

Hi! I m using uC STM32G491 and I have 2 ADC triggered by TIM1 CCR3. First ADC1 converts 1 channel and ADC2 converts 2 channels in scan mode. How can I know in which JDRy registers it will be stored each conversion result?

OIoni.1
Associate II

Conversion of ADC1 and first channel of ADC2 will finish theoretically at the same time.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Igor Cesko
ST Employee

Hi OIoni.1 ,

Each ADC has set of ADC_JDRy registers - where "y" is the conversion result in the injected sequence.

Example:

ADC1 converts only channel 4.

ADC2 converts in sequence channel 7 and the channel 3.

The result from ADC1 channel 4 is stored in ADC1_JDR1 (first converted in sequence).

The result from ADC2 channel 7 is stored in ADC2_JDR1 (first converted channel in sequence).

The result from ADC2 channel 3 is stored in ADC2_JDR2 (second converted channel in sequence).

Regards

Igor