2021-06-09 03:44 AM
After receiving some data through interrupt, Is there any way to disable interrupt mechanism and go back to blocking mode for receiving remaining data.
I tried NVIC_DisableIRQ(0 to disable interrupt.
After that when i tried to receive through blocking mode, it fails. I just need to know whether its possible in stm32?
2021-06-09 05:16 AM
Yes, blocking mode should work after using any of interrupt functions unless you've left the interrupt function unfinished
(not completed or canceled).
Also, disable RX overrun detection in UART initialization. It can cause problems.
But it is better to not use any HAL functions for UART, rather make your own.
--pa
2021-06-09 05:46 AM
2021-06-09 06:04 AM
Attached code not found.
2021-06-09 09:23 PM
2021-06-09 09:24 PM
2021-06-09 11:10 PM
Hi Pavel,
Can you please provide some solution for the attached code. I am using STM32H&A3 Nucleo board.
Thanks,
Jestina
2021-06-10 06:16 AM
Any update?
2021-06-10 07:25 AM
Hi @JJoy.1
Your code unfortunately has so many mistakes that IMHO it's hardly workable and beyond easy fix.
Calling HAL_UART_Receive_IT in the IRQ handler is very strange.
HAL_UART_RxCpltCallback looks strange too.
If this is a student assignment, request better documentation or examples from your teachers.
void USART3_IRQHandler(void)
{
/* USER CODE BEGIN USART3_IRQn 0 */
/* USER CODE END USART3_IRQn 0 */
HAL_UART_IRQHandler(&huart3);
/* USER CODE BEGIN USART3_IRQn 1 */
HAL_UART_Receive_IT(&huart3, status, 5);
/* USER CODE END USART3_IRQn 1 */
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
int j;
for(j =0; j <5; j++)
{
Serial_PutByte(status[j]);
resp =1;
}
NVIC_DisableIRQ(USART3_IRQn);
__HAL_UART_DISABLE_IT(&huart3,UART_IT_RXNE);
}
In any case I'd recommend disabling RX overflow. Change in MX_USART3_UART_Init
the line with huart3.AdvancedInit.AdvFeatureInit and add the next one:
static void MX_USART3_UART_Init(void)
{
.......
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_RXOVERRUNDISABLE_INIT;
huart3.AdvancedInit.OverrunDisable = UART_ADVFEATURE_OVERRUN_DISABLE;
if (HAL_UART_Init(&huart3) != HAL_OK)
....................
Good luck.
-- pa
2021-06-10 07:33 AM
Hi Pavel,
From where can i call the disabling function - NVIC_DisableIRQ(USART3_IRQn);
Jestina