2020-05-08 6:23 AM
As I said in the description, I would like use only one project instead of using 2 projects and. I've tried to use a single linker file and split it after the build using objcopy to obtain 2 separate binaries for internal and external flash, with no success.
Is there and example for this use case that I could use to see the correct setup? Maybe someone could help me with a simple Hello World example for this use case.
2020-05-08 4:09 PM
What exactly is your use case? What's stopping you from putting everything in the same project?
2020-05-10 11:25 PM
Hi, the use case is the following, the starting point was to use the examples from the template folder from SDK, program the internal Flash with the ExtMem_Boot and program the external memory with application, but using this configuration I need to use 2 separate projects, so I've tried to put everything in a single linker file, merge the source code and split the elf file generated in 2 separate binaries, one to be flashed in internal flash and one in external flash, is this the right way to do it ? Or there is other approach to do this?
I did not manage to make it working, that is why I was asking if there is a simple example, or if this is even possible to be done.