cancel
Showing results for 
Search instead for 
Did you mean: 

unable to program in stm32f7508dk

kishor
Associate II

sir we are getting this error while loading the code into stm32f7508 dk board

 

Error in final launch sequence:

 

Failed to execute MI command:

target remote localhost:60000

 

Error message from debugger back end:

Remote communication error. Target disconnected.: (undocumented errno 10061).

Failed to execute MI command:

target remote localhost:60000

 

Error message from debugger back end:

Remote communication error. Target disconnected.: (undocumented errno 10061).

Remote communication error. Target disconnected.: (undocumented errno 10061).

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

which CubeIDE version you are using?

If it’ the v1.15.0, did you try to update your stlink firmware?

See also this thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
mƎALLEm
ST Employee

Hello,

which CubeIDE version you are using?

If it’ the v1.15.0, did you try to update your stlink firmware?

See also this thread.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.