cancel
Showing results for 
Search instead for 
Did you mean: 

Hi all, I have a project that need to use NFC PN532 read / write Mifare Classic card with STM32F429Zi MCU communication via HSU. I'm in the initial stages of project, don't know what i should do, and what is the best path.Please help me.Thank you so much

Viet Quoc Dam
Associate

PN532 NFC/RFID module with STM32F429Zi communication via HSU

2 REPLIES 2
Ulysses HERNIOSUS
ST Employee

Hi,

ST25 NFC/RFID Tags and Readers is definitely the wrong topic here, removed it, adding STM32F4. But you are welcome to change to an ST25 solution. E.g. ST25R3916 + ST25TV (or ST25TA).

Br, Ulysses

Viet Quoc Dam
Associate

Oh I so sorry Br, Ulysses .This is my first time posting so there is a mistake in the post. My instructor did not agree to transfer, so I had to continue with the above topic. Can Br, Ulysses give me another opinion?

Thank you so much