2022-08-17 3:00 AM
2022-12-28 2:46 AM
Hello @WSief.1,
This typo is fixed in ES0499-Rev5.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-17 8:42 AM
Hi @WSief.1 and welcome to the Community :),
Thanks for your contribution
Could you please share the file where the bit 31 of ADC_CFGR1 register is mentioned in the library?
I checked all the header files under “STM32Cube_FW_U5_V1.1.1\Drivers\CMSIS\Device\ST\STM32U5xx\Include�? but I didn’t find the definition of 31 bit in ADC _CFGR1 register.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-18 1:21 AM
There is no definition in header files (missed information that the reset value of register is 0x80000000). After reset of uC this register is set to a value 0x80000000.
This value is mentioned in reference manual. Unfortunately i missed the message that this bit must be kept at reset value,
which is 1. The question is if this bit is JQDIS. JQDIS bit is mentioned in errata datashit (STM32U575xx and STM32U585xx device errata).
2022-08-25 8:35 AM
Hi @WSief.1 ,
Thank you for bringing this issue our attention.
The 31 bit in the ADC_CFGR register is reserved and by default set to 1.
I confirm that bits JQDIS and JQM are not available in STM32U5, so the Errata Sheet will be updated accordingly.
I reported this issue internally.
Internal ticket number: 133618 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-28 2:46 AM
Hello @WSief.1,
This typo is fixed in ES0499-Rev5.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.