2023-05-22 4:16 AM
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */
#ifdef __GNUC__
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
#define GETCHAR_PROTOTYPE int __io_getchar(void)
#else
#define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)
#define GETCHAR_PROTOTYPE int fgetc(FILE *f)
#endif
PUTCHAR_PROTOTYPE
{
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
GETCHAR_PROTOTYPE
{
uint8_t ch = 0;
/* Clear the Overrun flag just before receiving the first character */
__HAL_UART_CLEAR_OREFLAG(&huart2);
/* Wait for reception of a character on the USART RX line and echo this
* character on console */
HAL_UART_Receive(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, HAL_MAX_DELAY);
return ch;
}
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
setvbuf(stdin, NULL ,_IONBF, 0);
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
char str[80];
int i;
printf("Enter your family name: ");
scanf("%79s", str);
printf("Enter your age: ");
scanf("%d", &i);
printf("Mr. %s, %d years old.\n", str, i);
printf("Enter a hexadecimal number: ");
scanf("%x", &i);
printf("You have entered %#x (%d).\n", i, i);
}
Solved! Go to Solution.
2023-05-25 12:52 AM
It might help others to describe what the problem / solution was.
2023-05-25 1:13 AM
Thanks LCE for your message,
Actually i use Nucleo-STM32F303K8, so i used UART2 to communicate between PC and Nucleo. I used many ways to receive sth from pc like scanf or HAL_UART_Receive function, but it didn't work, although CUBE-IDE generate automatically PA2 as USART2-TX and PA3 as as USART2_RX, but only TX has the connection to ST-LINK. It means when i press a Key on my PC-keyboard, i had the Signal on board(checked whit oscilloscope), however not on Processor, so i had to define another PIN(PA15) as my UART2-RX and then when i checked with Multi meter the connection were there(connection between ST_LINK and Processor).
if you look at page 11 on this user manual you can clearly know what i mean.
happy to hear any comments from you