cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, My c code is generated from stm MAT-TARGET, but when I run main file of the IDE(Keil and stm32cubeide) nothing happens on the board. Just trying to run simple blink led model.

MAziz.1
Associate II

 I am using stm32 F746ZG Nucleo LQFP 144. I am using stm32 MAT-TARGET to generate c code from my simulink model.I have read in the provided pdf by the Stm MAT-TARGET that stmcubeide is not well supported by this. So I am using Keil V5. Now after generating the c code from simulink when I opens my keil project , and run the main file nothing happens on my board. I am new to this please guide me. All the c and h files are generated for the respective model in my ide target, but I think the main c file corresponding to the core folder is not linked with the model files.(.c and .h). Please guide me in this regard. Attached are the related files of my project.

0 REPLIES 0