2020-07-22 10:42 AM
#define RCC_CFGR *((long*)0x40023808)
#define RCC_CR *((long*)0x40023800)
#define RCC_AHB1ENR *((long*)0x40023830)
#define GPIOC_ODR *((long*)0x40020814)
#define GPIOA_MODER *((long*)0x40020000)
#define GPIOA_OTYPER *((long*)0x40020004)
#define GPIOA_AFRL *((long*)0x40020020)
#define GPIOA_AFRH *((long*)0x40020024)
#define GPIOA_IDR *((long*)0x40020010)
#define RCC_APB1ENR *((long*)0x40023840)
#define RCC_APB2ENR *((long*)0x40023844)
#define USART1_BRR *((long*)0x40011008)
#define USART1_SR *((long*)0x40011000)
#define USART1_DR *((long*)0x40011004)
#define USART1_CR1 *((long*)0x4001100C)
#define USART1_CR2 *((long*)0x40011010)
//APB clock frequency=16MHz
//no APB prescaler
int main(void){
int k,i=1;
RCC_APB2ENR=RCC_APB2ENR|0x10; //USART1 enable
RCC_AHB1ENR=0x1; //abilitazione clock GPIOA
RCC_CFGR=0x0;
RCC_CR=RCC_CR|0x1;
GPIOA_MODER=GPIOA_MODER|0x280000; //PA9(USART1 TX) e PA10(USART1 RX) in alternate function mode
GPIOA_AFRH=0x770; //PA9 e PA10 connected to USART1
USART1_BRR=USART1_BRR|0x8B; // fisso un baud rate pari a 115200 simb/s
//USART1_BRR=USART1_BRR|0x341; // fisso un baud rate pari a 9600 simb/s
USART1_CR1=USART1_CR1|0x200C;
k=USART1_SR;
USART1_DR ='C';
while((USART1_SR&0x40)!=(0x40));
USART1_DR ='I';
while((USART1_SR&0x40)!=(0x40));
USART1_DR ='A';
while((USART1_SR&0x40)!=(0x40));
USART1_DR ='O';
while((USART1_SR&0x40)!=(0x40));
}
2020-07-23 12:02 PM
Use predefined register and bit names. And this is how you send a single character:
while (!(USART1->SR & USART_SR_TXE));
USART1->DR = 'X';
2020-07-23 2:09 PM
> I didn't understand this:GPIOA_AFRH=(GPIOA_AFRH & ~0xFF0) | 0x770; // PA9/PA10 AF7
What looks like a dash before 0xFF0 is a tilde ~0xFF0 <---- It is better seen in bold font.
A 'feature" of the brain dead salesforce forum.
-- pa