2023-04-24 7:00 AM
Sub: Single wire communication is not working
Dear Sir
I developed Hw design and and now writing firmware for stm32L476 microcontroller. Requirement of project is Single wire communication. I chose STM32L476, the reason behind was single wire communication (SWMPI on Port B pin12) peripheral present in this microcontroller. I took Bit rate 100kBits/sec.I connected both boards using swmpi wire and ground pins. Problem is that single wire communication is not working. I am not able to receive data at receiver side board.
i used as below code snippet:
To Initialize SWMPI
hswpmi1.Instance = SWPMI1;
hswpmi1.Init.VoltageClass = SWPMI_VOLTAGE_CLASS_B;
hswpmi1.Init.BitRate = 19;
hswpmi1.Init.TxBufferingMode = SWPMI_TX_NO_SOFTWAREBUFFER;
hswpmi1.Init.RxBufferingMode = SWPMI_RX_NO_SOFTWAREBUFFER;
i am using API for communication
Receiver Side microcontroller:
char tx_data_buf[32];
while(1){
status = HAL_SWPMI_Receive(&hswpmi1,(uint32_t *)&obj_convrt.v, 1,100);
if(status== HAL_OK)
{
memset(tx_data_buf,0,32);
sprintf(&tx_data_buf[0],"<%x,%x,%x,%x>\n", obj_convrt.b[0],obj_convrt.b[1], obj_convrt.b[2], obj_convrt.b[3]);
HAL_UART_Transmit_IT(&huart1,(uint8_t *)tx_data_buf,4);
}
}
Transmitter side Microcontroller:
uint32_t tx_swmpi_data = 0x12345678;
while(1){
HAL_SWPMI_Transmit(&hswpmi1,(uint32_t *)&tx_swmpi_data,1,100);
HAL_Delay(1000);
}
Please help in this regards . I have also attached hardware schematic snap shots
2023-04-24 7:10 AM - edited 2023-11-20 7:18 AM
Sub: Single wire communication is not working
Dear Sir
I developed Hw design and and now writing firmware for stm32L476 microcontroller. Requirement of project is Single wire communication. I chose STM32L476, the reason behind was single wire communication (SWMPI on Port B pin12) peripheral present in this microcontroller. I took Bit rate 100kBits/sec.I connected both boards using swmpi wire and ground pins. Problem is that single wire communication is not working. I am not able to receive data at receiver side board.
i used as below code snippet:
To Initialize SWMPI
hswpmi1.Instance = SWPMI1;
hswpmi1.Init.VoltageClass = SWPMI_VOLTAGE_CLASS_B;
hswpmi1.Init.BitRate = 19;
hswpmi1.Init.TxBufferingMode = SWPMI_TX_NO_SOFTWAREBUFFER;
hswpmi1.Init.RxBufferingMode = SWPMI_RX_NO_SOFTWAREBUFFER;
i am using API for communication
Receiver Side microcontroller:
char tx_data_buf[32];
while(1){
status = HAL_SWPMI_Receive(&hswpmi1,(uint32_t *)&obj_convrt.v, 1,100);
if(status== HAL_OK)
{
memset(tx_data_buf,0,32);
sprintf(&tx_data_buf[0],"<%x,%x,%x,%x>\n", obj_convrt.b[0],obj_convrt.b[1], obj_convrt.b[2], obj_convrt.b[3]);
HAL_UART_Transmit_IT(&huart1,(uint8_t *)tx_data_buf,4);
}
}
Transmitter side Microcontroller:
uint32_t tx_swmpi_data = 0x12345678;
while(1){
HAL_SWPMI_Transmit(&hswpmi1,(uint32_t *)&tx_swmpi_data,1,100);
HAL_Delay(1000);
}
Please help in this regards . I have also attached hardware schematic snap shots
2023-04-24 7:14 AM
Define "not working"
Perhaps use a scope or logic analyzer to review signals and contrast against expected signals.
Your UART transmit doesn't seem to output enough data
2023-04-24 7:22 AM
Thanks for reply.
I am sending data one WORD size. with value 0x12345678 from one board as Transmitter unit ;
And Other MCU board Unit as Receiver to read data from SWMPI single wire communication.
But I got value as 0x00 00 00 00 , as four bytes. I also used Oscilloscope to view data pattern.
2023-04-24 9:45 AM
Perhaps try some of the examples, and test functionality of those, port to your platform
STM32Cube_FW_L4_V1.17.2\Projects\STM32L476G-EVAL\Examples\SWPMI\SWPMI_Session\Src\main.c
Find an FAE in your local sales office to discuss this with. Not sure there's much support of SWPMI here, or many with own hardware.