2021-01-28 5:10 AM
I want to update the firmware and my micro is a single bank flash memory.
Is it possible to do a firmware update with this micro ??
Or should it be dual bank flash memory ??
Can I use AT45DB321 as a second memory bank ??
2021-01-30 11:47 PM
Hello. Can anyone help me?
2021-01-31 4:01 AM
You haven't even mentioned the MCU...
Start with learning some basics:
After that continue to reading AN4657 as an example and AN2606.
2021-01-31 11:33 PM
Thanks for your tips