Handling 16bit register address in i2c communication
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-05 5:43 AM
I am trying to use ov5640 camera with stm32l4r5 board nucleo-144. The ov5640 has SCCB bus which is similar to i2c. But ov5640 has register with 16bit address (0x300A, 0x300B like this). I used CUBEMX to initialise i2c pins and generated code. How can I communicate with camera using i2c. I am using following code but it is not working.
int ov5640_init(I2C_HandleTypeDef *p_hi2c)
{
sp_hi2c = p_hi2c;
int returnValue = 0;
uint8_t buffer;
//ov5640_write(0x31, 0x11);
//reg = ov5640_write(0x3008, 0x82);
HAL_Delay(30);
returnValue = ov5640_read(OV5640_CHIPIDH, &buffer);
if (buffer == 0x56)
{
returnValue = ov5640_read(OV5640_CHIPIDL, &buffer);
if (buffer == 0x40)
{
return 0;
}
else
{
return 1;
}
}
else
{
return 1;
}
}
static int ov5640_write(uint16_t regAddr, uint8_t data)
{
HAL_StatusTypeDef ret;
do {
ret = HAL_I2C_Mem_Write(sp_hi2c, OV5640_WR_ADDR, regAddr, I2C_MEMADD_SIZE_16BIT, &data, 1, 100);
} while (ret != HAL_OK && 0);
return ret;
}
static int ov5640_read(uint16_t regAddr, uint8_t *data)
{
HAL_StatusTypeDef ret;
uint8_t regAddrMSB = regAddr >> 8;
uint8_t regAddrLSB = regAddr & 0xFF;
do {
ret = HAL_I2C_Master_Transmit(sp_hi2c, 0x78, ®AddrMSB, 1, 100);
ret |= HAL_I2C_Master_Transmit(sp_hi2c, 0x78, ®AddrLSB, 1, 100);
ret |= HAL_I2C_Master_Receive(sp_hi2c, 0x79, data, 1, 100);
} while (ret != HAL_OK && 0);
return ret;
}
Solved! Go to Solution.
- Labels:
-
I2C
-
STM32L4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-05 6:55 AM
hello
Device slave address sould be shifted left by one bit,
A way to read data from a 16 bit address is
HAL_I2C_Mem_Read(sp_hi2c, 0x78<<1, regAddr, 2, data, datalen, timeout);
regAddr is 16 bit address and "2" is the size in bytes of regAddr.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-05 6:55 AM
hello
Device slave address sould be shifted left by one bit,
A way to read data from a 16 bit address is
HAL_I2C_Mem_Read(sp_hi2c, 0x78<<1, regAddr, 2, data, datalen, timeout);
regAddr is 16 bit address and "2" is the size in bytes of regAddr.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-05 11:10 PM
Thanks your suggestion worked for me. HAL_I2C_Mem_Read worked.