2019-03-08 8:40 AM
According to ARM Cortex-A Series Programmer’s Guide for ARMv8-A:
15.1.2. Standby
...
This mode is entered using either the WFI (Wait For Interrupt) or WFE (Wait For Event) instructions. ARM recommends the use of a Data Synchronization Barrier (DSB) instruction before WFI or WFE, to ensure that pending memory transactions complete before changing state.
--> The HAL function HAL_PWR_EnterSLEEPMode() does not perform the DSB instruction before the WFE or WFI instruction. I believe that this is an error in the HAL code.
2019-03-09 4:53 AM
While the main point is correct, one should refer to Cortex-M documentation, not Cortex-A.
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dai0321a/BIHICBGB.html
ST's developers are systematically ignoring needed memory barriers everywhere. That's one of the reasons their ETH/lwIP drivers are so flawed that they are basically non-working. Now on a fast Cortex-M7 based MCUs it is showing off in it's full glory of instability. And it has been reported in this forum multiple times years ago...