2015-11-14 2:22 AM
Hello, I'm trying to communicate with a STM32f4x9 EVAL board and a STM32F429-Discovery board via CAN Bus,
I am using MCP2551 transceiver IC for Discovery board, I know that CAN1 is being used by LCD and CAN2 is used by USB OTG. So I de-soldered the C53 (4k7 uf) capacitor of Discovery board (according to a video onhttps://www.youtube.com/watch?v=4fYoXGiIdDs
), I have tested everything, wirings, HAL configs for CAN, etc.. But I'm getting timeout when I call the HAL_CAN_Transmit function. I am using pure STMCube examples (STM32F4x9_EVAL\Examples\CAN\CAN_Networking), I re-configured the same example for Discovery board, using CAN2 instead of CAN1. Here is my wiring schematic:bool CANWorker::init_HAL_CAN()
{
// Placed in MCP file:
GPIO_InitTypeDef GPIO_InitStruct;
/*##-1- Enable peripherals and GPIO Clocks #################################*/
/* CAN2 Periph clock enable */
CANx_CLK_ENABLE();
/* Enable GPIO clock ****************************************/
CANx_GPIO_CLK_ENABLE();
/*##-2- Configure peripheral GPIO ##########################################*/
/* CAN2 TX GPIO pin configuration */
GPIO_InitStruct.Pin = CANx_TX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Alternate = CANx_TX_AF;
HAL_GPIO_Init(CANx_TX_GPIO_PORT, &GPIO_InitStruct);
/* CAN2 RX GPIO pin configuration */
GPIO_InitStruct.Pin = CANx_RX_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FAST;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Alternate = CANx_RX_AF;
HAL_GPIO_Init(CANx_TX_GPIO_PORT, &GPIO_InitStruct);
/*##-3- Configure the NVIC #################################################*/
/* NVIC configuration for CAN2 Reception complete interrupt */
HAL_NVIC_SetPriority(CANx_RX_IRQn, 1, 0);
HAL_NVIC_EnableIRQ(CANx_RX_IRQn);
CAN_FilterConfTypeDef sFilterConfig;
static CanTxMsgTypeDef TxMessage;
static CanRxMsgTypeDef RxMessage;
/*##-1- Configure the CAN peripheral #######################################*/
_canHandle.Instance = CAN2;
_canHandle.pTxMsg = &TxMessage;
_canHandle.pRxMsg = &RxMessage;
_canHandle.Init.TTCM = DISABLE;
_canHandle.Init.ABOM = DISABLE;
_canHandle.Init.AWUM = DISABLE;
_canHandle.Init.NART = DISABLE;
_canHandle.Init.RFLM = DISABLE;
_canHandle.Init.TXFP = DISABLE;
_canHandle.Init.Mode = CAN_MODE_NORMAL;
_canHandle.Init.SJW = CAN_SJW_1TQ;
_canHandle.Init.BS1 = CAN_BS1_6TQ;
_canHandle.Init.BS2 = CAN_BS2_8TQ;
_canHandle.Init.Prescaler = 2;
if(HAL_CAN_Init(&_canHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
return false;
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterNumber = 14;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if(HAL_CAN_ConfigFilter(&_canHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
return false;
}
/*##-3- Configure Transmission process #####################################*/
_canHandle.pTxMsg->StdId = 0x321;
_canHandle.pTxMsg->ExtId = 0x01;
_canHandle.pTxMsg->RTR = CAN_RTR_DATA;
_canHandle.pTxMsg->IDE = CAN_ID_STD;
_canHandle.pTxMsg->DLC = 2;
return true;
}
void HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* CanHandle)
{
if ((CanHandle->pRxMsg->StdId == 0x321)&&(CanHandle->pRxMsg->IDE == CAN_ID_STD) && (CanHandle->pRxMsg->DLC == 2))
{
LED_Display(CanHandle->pRxMsg->Data[0]);
ubKeyNumber = CanHandle->pRxMsg->Data[0];
}
/* Receive */
if(HAL_CAN_Receive_IT(CanHandle, CAN_FIFO0) != HAL_OK)
{
/* Reception Error */
//Error_Handler();
}
}
CANWorker::CANWorker ()
{
init_HAL_CAN();
BSP_PB_Init(BUTTON_KEY, BUTTON_MODE_GPIO);
/*##-2- Start the Reception process and enable reception interrupt #########*/
if(HAL_CAN_Receive_IT(&_canHandle, CAN_FIFO0) != HAL_OK)
{
/* Reception Error */
Error_Handler();
}
/* Infinite loop */
while(1)
{
while(BSP_PB_GetState(BUTTON_KEY) == KEY_PRESSED)
{
if(ubKeyNumber == 0x4)
{
ubKeyNumber = 0x00;
}
else
{
LED_Display(++ubKeyNumber);
/* Set the data to be transmitted */
_canHandle.pTxMsg->Data[0] = ubKeyNumber;
_canHandle.pTxMsg->Data[1] = 0xAD;
/*##-3- Start the Transmission process ###############################*/
if(HAL_CAN_Transmit(&_canHandle, 1000) != HAL_OK)
{
/* Transmition Error */
Error_Handler();
}
HAL_Delay(10);
while(BSP_PB_GetState(BUTTON_KEY) != KEY_NOT_PRESSED)
{
}
}
}
}
}
But the ''HAL_CAN_Transmit'' returns timeout, waiting for TransmitMailbox to be sent (Following codes are from : stm32f4xx_hal_can.c
/* Check End of transmission flag */
while(!(__HAL_CAN_TRANSMIT_STATUS(hcan, transmitmailbox)))
{
/* Check for the Timeout */
if(Timeout != HAL_MAX_DELAY)
{
if((Timeout == 0)||((HAL_GetTick() - tickstart ) > Timeout))
{
hcan->State = HAL_CAN_STATE_TIMEOUT;
/* Process unlocked */
__HAL_UNLOCK(hcan);
return HAL_TIMEOUT;
}
}
}
What am I doing wrong? It's not because I use a MCP2551 and the EVAL board is using HVD230 transceiver instead, right?
It seems that the other not does not ACK the sent frame, am I right? What causes this?
#transmission #stm32 #stm32f4 #can #can #error #timeout #can-timeout
2015-11-15 11:36 PM
Please help me! I can't figure out the problem...
2015-11-16 4:48 AM
Check the CAN ESR register on both sides. It will tell you what the error code is.
Jack Peacock2015-11-19 3:38 AM
Hello, i have the same problem.
Did you find
the solution
?can you explain me please?
2015-12-01 4:10 AM
Well, the timeout problem was a physical link issue, I don't remember what it was exactly (maybe the MCP2551s where broken, because I changed them), however, it is working right now.
I also tried without using transceiver ICs, page 4 of this document : http://www.keil.com/appnotes/files/apnt_236.pdf and it worked fine.The problem I still have, is that I can not use CAN2, receive interrupts are not called, so I changed my code to use CAN1.I you still have problem, put your configurations and codes, maybe I can help you :)2016-01-28 3:50 PM
For anyone who is trying to read a car ECU CAN data, here is a handy github gist
(A guide how to automate the baudrate calculating for CAN bus)2017-12-26 3:25 PM
I'm getting the same timeout error at the same location. I've ported the CAN Networking sample over from the eval board sample sources to the STM32f303re. I can send a packet and it appears to get to the 2nd STM32 across the CAN bus based on looking at the TX and RX lines on the 2 devices but it never seems to trigger the CAN TX or RX interrupts. I see that the 303 has different interrupts than the eval board processor and I've tried to map them correctly but so far have had no luck.
Has anyone succeeded at getting CAN working on the STM32F303re?
2017-12-26 6:44 PM
is Rx or Tx not running ?
I have CAN working on '091 and '767
I started by receiving packets from an external CanDo unit. then I worked on transmission.
I couldn't get the examples to work either.
I use the HAL Callbacks;
void CEC_CAN_IRQHandler(void)
{ /* USER CODE BEGIN CEC_CAN_IRQn 0 */ CAN_IRQFlag = true; checkCanRxFifos();/* USER CODE END CEC_CAN_IRQn 0 */
HAL_CAN_IRQHandler(&hcan); /* USER CODE BEGIN CEC_CAN_IRQn 1 *//* USER CODE END CEC_CAN_IRQn 1 */
}2017-12-27 12:27 PM
It appears the TX is 'working'. In quotes because I see a repeatable waveform on the CAN bus when I press the button which triggers the send. The packet is exactly from the CAN Networking sample. But, I never get any TX or RX callbacks or interrupts from the CAN routines. The main.h file (below) declares the RX IRQs but not the TX IRQs. Also, I'm not sure what the AF9_CAN gpio pin is used for or if that pin needs to be changed for the 303re part.
/* Exported types ------------------------------------------------------------*/
/* Exported constants --------------------------------------------------------*//* User can use this section to tailor CANx instance used and associated resources *//* Definition for CANx clock resources */ ♯ define CANx CAN1 ♯ define CANx_CLK_ENABLE() __HAL_RCC_CAN1_CLK_ENABLE() ♯ define CANx_GPIO_CLK_ENABLE() __HAL_RCC_GPIOD_CLK_ENABLE() ♯ define CANx_FORCE_RESET() __HAL_RCC_CAN1_FORCE_RESET() ♯ define CANx_RELEASE_RESET() __HAL_RCC_CAN1_RELEASE_RESET()/* Definition for USARTx Pins */
♯ define CANx_TX_PIN GPIO_PIN_11 ♯ define CANx_TX_GPIO_PORT GPIOA ♯ define CANx_TX_AF GPIO_AF9_CAN ♯ define CANx_RX_PIN GPIO_PIN_12 ♯ define CANx_RX_GPIO_PORT GPIOA ♯ define CANx_RX_AF GPIO_AF9_CAN/* Definition for USARTx's NVIC */
♯ define CANx_RX_IRQn CAN_RX0_IRQn ♯ define CANx_RX_IRQHandler CAN_RX0_IRQHandlerI must say the whole CAN subsystem and HAL implementation is very opaque to me. I feel like I'm stumbling around in the dark. Is there any documentation describing this? I know the eval board (the source of the networking sample code) has individual interrupts for CAN and it appears the 303re uses an interrupt that handles both USB and CAN. We're not using USB on this product but on some forum post someone indicated that you needed to initialize USB before initializing CAN? Any ideas?
Waiting for the CAN light to illuminate....
2017-12-27 3:50 PM
with or without USB, my CAN works fine.
can you receive in the dongle, the CAN packet that you sent from the EVAL?
please make sure that you are not sending the same 'ID' from both boards.
this will cause the canbus to go into an error state, then nothing will work correctly until you power cycle the board set.
this is my startup
void initCairoCan (void) {
CAN_Config(); canRxpointerIN = 0; canRxMsgIN =0; canRxMsgOUT =0; canRxMsgTableEMPTY = true; canRxMsgTableFULL = false;for(int i = 0; i<16;i++)
IOCanMsgFlag[i] =false;// // Receive Interrupts ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FF0); //!< FIFO 0 full interrupt ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FOV0); //!< FIFO 0 overrun interrupt ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FF1); //!< FIFO 1 full interrupt ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FOV1); //!< FIFO 1 overrun interrupt ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FMP0); //!< FIFO 0 message pending interrupt ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_FMP1); //!< FIFO 1 message pending interrupt ////// // Operating Mode Interrupts ////// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_WKU); //!< Wake-up interrupt //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_SLK); //!< Sleep acknowledge interrupt //////// // Error Interrupts //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_EWG); //!< Error warning interrupt //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_EPV); //!< Error passive interrupt //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_BOF); //!< Bus-off interrupt //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_LEC); //!< Last error code interrupt //// __HAL_CAN_ENABLE_IT(&hcan1, CAN_IT_ERR); //!< Error Interrupt //// /* Enable Transmit mailbox empty Interrupt */ __HAL_CAN_ENABLE_IT (&hcan1, CAN_IT_TME); //!< Transmit mailbox empty interrupt // __HAL_CAN_ENABLE_IT (&hcan1, CAN_IT_FMP0); //!< FIFO 0 message pending interrupt // __HAL_CAN_ENABLE_IT (&hcan1, CAN_IT_FMP1); //!< FIFO 1 message pending interrupt //canTxMsgIN =0;
canTxMsgOUT =0; canTxMsgTableEMPTY = true; canTxMsgTableFULL = false; canTxMsgTableOverflow = false; canTxMsgOverrun = false; blockCanTx = false;}