cancel
Showing results for 
Search instead for 
Did you mean: 

H743ZI Full-duplex DMA communication. When the baud rate is 25M, the master and the slave can receive the data correctly. When 50M and 100M, the slave can receive the data correctly, but the master cannot receive the data correctly.

one V
Associate III

Use two NUCLEO-H743ZI boards for SPI communication. Full-duplex DMA mode. When the baud rate is 25M, the master and the slave can receive the data correctly. At 50M and 100M, the slave can receive the data correctly, but the master cannot receive the data correctly. Why?

1 REPLY 1
TDK
Guru

Sounds like a signal integrity issue. 100 MHz is high for transfers between boards connected by jumper wires.

If you feel a post has answered your question, please click "Accept as Solution".