2025-02-12 04:42 PM
Hello,
I started a new project using the H743, ethernet, LAN8742 and NetXDuo (on one of our custom boards). Its a very simple project that initializes the hardware, initializes AzRtos, ThreadX, and NetXDuo, and starts TCP, UDP, and ICMP. This project is just a base (Starting point) for much bigger projects. When connected to the network, i can ping the board, it can either use a static IP or the DHCP client.
The strange part is that the software works when the clock configuration is set to 400MHz. If I try to set it to 480MHz, NetXDuo doesn't receive any packets from the network. At 480MHz, the phy is working properly and it detects (prints a line) stating the status of the ethernet cable (plugged in / unplugged). The phy is sending a 50mhz clock to the H743, so I don't understand why the MCU works at 400 but not 480. Anyway, I've been pulling my hair out trying to figure out why it doesn't work. Everything in the Clock Configuration looks ok and CubeIDE does not complain about any of the values entered. Does anyone have any clue or suggestions as to why it doesn't work at 480MHz?
Thanks
Matthew
2025-02-12 10:32 PM
2025-02-12 10:37 PM
Hi @mbarg.1
I found an errata that says there is a hardware problem with some revisions of this chip. Cannot go above 400MHz...
I think we recently purchased these chips from distribution....
Matthew
2025-02-12 10:52 PM
kudos and solution accepted are always welcome - thanks
2025-02-12 11:18 PM
Hi @mbarg.1
I escalated the issue to ST engineers, but it seems their Errata is wrong. I'll wait to hear back from them before sending you a kudos :)
thanks
Matt
2025-02-13 12:45 AM
I usually check for counterfait devices in SFRs.
my devices are
2025-02-13 03:04 AM - edited 2025-02-13 03:58 AM
Hello,
As it's generated with CubeMx/CubeIDE I don't think there is an issue in the clock config and indeed rev V can reach 480MHz with VOS0.
I'm not expert of ETH but does the product run with a simple example at 480MHz? What is the product package are you using?
See also this errata:
2025-02-13 03:59 AM
@SofLit wrote:
See also this errata:
Ok I see you are using LAN8742 (RMII) so you are not in this errata ..