cancel
Showing results for 
Search instead for 
Did you mean: 

H743 ethernet clocking issue

matt-crc
Associate

Hello,

I started a new project using the H743, ethernet, LAN8742 and NetXDuo (on one of our custom boards).  Its a very simple project that initializes the hardware, initializes AzRtos, ThreadX, and NetXDuo, and starts TCP, UDP, and ICMP.  This project is just a base (Starting point) for much bigger projects.  When connected to the network, i can ping the board, it can either use a static IP or  the DHCP client.

The strange part is that the software works when the clock configuration is set to 400MHz.  If I try to set it to 480MHz, NetXDuo doesn't receive any packets from the network.  At 480MHz, the phy is working properly and it detects (prints a line) stating the status of the ethernet cable (plugged in / unplugged). The phy is sending a 50mhz clock to the H743, so I don't understand why the MCU works at 400 but not 480.   Anyway, I've been pulling my hair out trying to figure out why it doesn't work.  Everything in the Clock Configuration looks ok and CubeIDE does not complain about any of the values entered.  Does anyone have any clue or suggestions as to why it doesn't work at 480MHz?

Thanks

Matthew

5 REPLIES 5
mbarg.1
Senior

I am currently running several projects all @480mhz, and they all perform 100%.

I share an .ioc file that you can compare with your setup.

There is no reason why it should not work BUT some early nucleo boards had beta devices limited to 300 MHz - check your hw,

 

Hi @mbarg.1 

I found an errata that says there is a hardware problem with some revisions of this chip.  Cannot go above 400MHz...

mattcrc_0-1739428556645.png

I think we recently purchased these chips from distribution....  

Matthew

kudos and solution accepted are always welcome - thanks

Hi @mbarg.1 

I escalated the issue to ST engineers, but it seems their Errata is wrong.  I'll wait to hear back from them before sending you a kudos :) 

mattcrc_0-1739431044305.png

thanks

Matt

I usually check for counterfait devices in SFRs.

my devices are

mbarg1_0-1739436306787.png