Skip to main content
Louie88
Senior
April 1, 2022
Question

H723ZG Nucleo ADC clock/noise question

  • April 1, 2022
  • 13 replies
  • 7681 views

After assembling the X3 external 25MHz crystal and 2 caps and generating initialize code for 550MHz clock with CubeMX my NUCLEO-H723ZG board runs fine, except ADC. It is very noisy. The CubeMX configured the clock for ADC = 96.000671 MHz (PLL2P). In the datasheet of the MCU the maximum ADC clock is 50MHz (BOOST=3) Is this okay or I found a bug in CubeMX?

I use ADC1 and ADC2 to sample two 150Hz 2Vpp sine wave signals. There is 100us phase difference between signals. (Blue is delayed) I start the ADCs simultaneously from TIMER1. When HAL_ADC_ConvCpltCallback() is called I read the ADC1 (yellow) and ADC2 (bule) conversion results. I generate the ADC1 – ADC2 signal with DAC1. Because the ADCs are in 16-bit mode but the DAC1 can handle 12-bit numbers only I right shift the ADC result by 4 and subtract the 12-bit numbers.

uint32_t difference = (chn1Data >> 4) - (chn2Data >> 4);

I write the value of difference variable into the DAC1. This is the green channel.

0693W00000Lwc7AQAR.bmp

  • Yellow: A signal (1V)
  • Blue: B signal (1V)
  • Orange: Comparator output (1V) It compares A input signal to +1.25V.
  • Green: A-B signal on output of 12-bit DAC1 (100mV)

I also tried the 64-bit oversampling but it did not help or I configured something faulty:

 hadc1.Init.OversamplingMode = ENABLE;
 hadc1.Init.Oversampling.Ratio = 1 << 6;
 hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_6;
 hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
 hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_RESUMED_MODE; 

With these settings I could get back the (integer) average of 64 ADC conversions of every sample point. Am I right?

Anybody has any idea why the difference signal so terrible?

Thanks,

Louis

This topic has been closed for replies.

13 replies

Pavel A.
May 3, 2022
Louie88
Louie88Author
Senior
May 4, 2022

Thanks Pavel for the link. I will check it.

Louis