2025-03-14 7:14 AM - edited 2025-03-15 4:06 PM
I am using this MCU on a battery-supplied custom board: STM32G0B1RET.
I am looking for clarification re. the GPIO availability in Standby Mode.
Table 26 in Reference Manual RM0444 (see below) seems to offer one of two (exclusive) possibilities:
Please confirm. Thank you!
2025-03-16 12:04 PM
Try RM0444 chapter 7.3.15, but yes isnt very clean.
2025-03-16 9:32 PM
@TDK, just for clarification re. the STM32G0B1RET on a battery-supplied custom board: the datasheet states that the pull-down resistor is weak, Table 55 lists around 40kOhm (see below). Can that cause a problem in Standby mode?
Also, one member states that in Standby Mode only RTC pins can drive low.
Please advise, I look forward to resolving this.
2025-03-17 4:42 AM
I don't see why that would cause a problem.
Not sure, no board here for me to test. Seems like it should work.